<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 How to interface freescale K81 with i.MX6?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-interface-freescale-K81-with-i-MX6/m-p/608076#M91704</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For one of my application it requires to interface freescale K81 MCU with i.MX6 over SPI interface.&lt;/P&gt;&lt;P&gt;Do I need to write the driver for communication between these devices ?&lt;/P&gt;&lt;P&gt;If yes then please suggest some driver names for reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Hrushi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Oct 2016 05:06:40 GMT</pubDate>
    <dc:creator>hrushinale</dc:creator>
    <dc:date>2016-10-05T05:06:40Z</dc:date>
    <item>
      <title>How to interface freescale K81 with i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-interface-freescale-K81-with-i-MX6/m-p/608076#M91704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For one of my application it requires to interface freescale K81 MCU with i.MX6 over SPI interface.&lt;/P&gt;&lt;P&gt;Do I need to write the driver for communication between these devices ?&lt;/P&gt;&lt;P&gt;If yes then please suggest some driver names for reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Hrushi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Oct 2016 05:06:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-interface-freescale-K81-with-i-MX6/m-p/608076#M91704</guid>
      <dc:creator>hrushinale</dc:creator>
      <dc:date>2016-10-05T05:06:40Z</dc:date>
    </item>
    <item>
      <title>Re: How to interface freescale K81 with i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-interface-freescale-K81-with-i-MX6/m-p/608077#M91705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hrushi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to adapt imx-test (folder /mxc_spi_test)&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz"&gt;www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;just for reference one can also look at attached Linux Manual&lt;/P&gt;&lt;P&gt;Chapter 31 SPI NOR Flash Memory Technology Device (MTD) Driver&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Oct 2016 06:15:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-interface-freescale-K81-with-i-MX6/m-p/608077#M91705</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-05T06:15:27Z</dc:date>
    </item>
  </channel>
</rss>