<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Configured as digital input pin do not change value ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Configured-as-digital-input-pin-do-not-change-value/m-p/608071#M91701</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nirmal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can attach jtag and check gpio registers described in&lt;/P&gt;&lt;P&gt;i.MX6UL Reference Manual Chapter 4 External Signals and Pin Multiplexing,&lt;/P&gt;&lt;P&gt;Chapter 26 General Purpose Input/Output (GPIO)&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;for uboot one can look at variscite resources&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/varigit" title="https://github.com/varigit"&gt;Variscite · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Apr 2017 00:03:55 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-04-14T00:03:55Z</dc:date>
    <item>
      <title>Configured as digital input pin do not change value ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configured-as-digital-input-pin-do-not-change-value/m-p/608070#M91700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using DART 6UL CPU for one of my custom board&lt;/P&gt;&lt;P&gt;ref: &lt;A class="link-titled" href="http://www.variscite.com/products/system-on-module-som/cortex-a7/dart-6ul-freescale-imx-6ul" title="http://www.variscite.com/products/system-on-module-som/cortex-a7/dart-6ul-freescale-imx-6ul"&gt;DART-6UL CPU: NXP/Freescale i.MX 6UltraLite / i.MX 6ULL - Variscite&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to configure 8 Digital Input pins out of which I have successfully configured 7.&lt;/P&gt;&lt;P&gt;But I am not able to drive GPIO1_0 as an input pin.&lt;/P&gt;&lt;P&gt;I removed GPIO1_0 from my dtsi file, in order to make it usable from user space.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can configure pin as input using&lt;/P&gt;&lt;P&gt;echo 0 &amp;gt; /sys/class/gpio/export&lt;/P&gt;&lt;P&gt;echo in &amp;gt; /sys/class/gpio/gpio0/direction&lt;/P&gt;&lt;P&gt;and it also appears in the /sys/kernel/debug/gpio list.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But it do not change its value when driven high or low.&lt;/P&gt;&lt;P&gt;Can anybody help me out here ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Questions :&lt;/P&gt;&lt;P&gt;1. What could be possible cause ?&lt;/P&gt;&lt;P&gt;2. If uboot source could the reason , where i can find source file and where to look for it ?&lt;/P&gt;&lt;P&gt;3. Is there anyother way I can free the pin, to make sure it is not configured by kernel !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Apr 2017 14:39:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configured-as-digital-input-pin-do-not-change-value/m-p/608070#M91700</guid>
      <dc:creator>nirmalpanchal</dc:creator>
      <dc:date>2017-04-13T14:39:20Z</dc:date>
    </item>
    <item>
      <title>Re: Configured as digital input pin do not change value ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configured-as-digital-input-pin-do-not-change-value/m-p/608071#M91701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nirmal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can attach jtag and check gpio registers described in&lt;/P&gt;&lt;P&gt;i.MX6UL Reference Manual Chapter 4 External Signals and Pin Multiplexing,&lt;/P&gt;&lt;P&gt;Chapter 26 General Purpose Input/Output (GPIO)&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;for uboot one can look at variscite resources&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/varigit" title="https://github.com/varigit"&gt;Variscite · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Apr 2017 00:03:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configured-as-digital-input-pin-do-not-change-value/m-p/608071#M91701</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-14T00:03:55Z</dc:date>
    </item>
  </channel>
</rss>