<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IPUv3 in EBoot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IPUv3-in-EBoot/m-p/608051#M91699</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;WinCE for i.MX6 is not supported by NXP directly. Please apply to Witekio / Adeneo.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;A class="link-titled" href="http://witekio.com/cpu/i-mx-6/" title="http://witekio.com/cpu/i-mx-6/"&gt;i.MX 6 - Witekio&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Sep 2016 07:20:47 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-09-27T07:20:47Z</dc:date>
    <item>
      <title>IPUv3 in EBoot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPUv3-in-EBoot/m-p/608050#M91698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am bringing up a SABRE like board which is fitted with handset(i.e. portrait orientation) LCD on an RGB interface. Our application is landscape mode, so can I use the IRT to rotate all my EBoot output i.e. splash screens, boot menus etc ?&lt;/P&gt;&lt;P&gt;If so then how do I plumb it in ? All the application notes I can find re rotation are for use at the OS level.&lt;/P&gt;&lt;P&gt;It seems I'd need to modify the&amp;nbsp;function 'DisplayConfigure' in SRC\BOOTLOADER\DISPLAY\ebootdisplay.c of the SabreBSP to setup the IRT DMA channels and plumb them into the image data flow?&lt;/P&gt;&lt;P&gt;(I come from an embedded MCU programming background so this SOC programming is upping the game a bit!)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THx,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Sep 2016 02:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPUv3-in-EBoot/m-p/608050#M91698</guid>
      <dc:creator>chrisbayley</dc:creator>
      <dc:date>2016-09-12T02:37:21Z</dc:date>
    </item>
    <item>
      <title>Re: IPUv3 in EBoot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPUv3-in-EBoot/m-p/608051#M91699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;WinCE for i.MX6 is not supported by NXP directly. Please apply to Witekio / Adeneo.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;A class="link-titled" href="http://witekio.com/cpu/i-mx-6/" title="http://witekio.com/cpu/i-mx-6/"&gt;i.MX 6 - Witekio&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 07:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPUv3-in-EBoot/m-p/608051#M91699</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-27T07:20:47Z</dc:date>
    </item>
  </channel>
</rss>