<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6 Camera driver porting  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Camera-driver-porting/m-p/607724#M91663</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am the beginner of the camera drivers .&lt;/P&gt;&lt;P&gt;Currently i am using imx6 &amp;nbsp;board , i am using the ov5640 mipi camera device.&lt;/P&gt;&lt;P&gt;IMX6 in Boundary device source code i browsed inside the code TWO MIPI CSI Drivers is avilable.&lt;/P&gt;&lt;P&gt;one is for &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;:&amp;nbsp;drivers/media/platform/mxc/capture &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;second one is for : drivers/media/platform/mxc/subdev&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am confusing which one is the correct driver .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Viswa&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Apr 2017 11:17:12 GMT</pubDate>
    <dc:creator>viswanathreddy</dc:creator>
    <dc:date>2017-04-13T11:17:12Z</dc:date>
    <item>
      <title>IMX6 Camera driver porting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Camera-driver-porting/m-p/607724#M91663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am the beginner of the camera drivers .&lt;/P&gt;&lt;P&gt;Currently i am using imx6 &amp;nbsp;board , i am using the ov5640 mipi camera device.&lt;/P&gt;&lt;P&gt;IMX6 in Boundary device source code i browsed inside the code TWO MIPI CSI Drivers is avilable.&lt;/P&gt;&lt;P&gt;one is for &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;:&amp;nbsp;drivers/media/platform/mxc/capture &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;second one is for : drivers/media/platform/mxc/subdev&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am confusing which one is the correct driver .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Viswa&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Apr 2017 11:17:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Camera-driver-porting/m-p/607724#M91663</guid>
      <dc:creator>viswanathreddy</dc:creator>
      <dc:date>2017-04-13T11:17:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Camera driver porting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Camera-driver-porting/m-p/607725#M91664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Viswa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;subdev driver is used for new processors like i.MX6UL, 7D with PxP, CMOS Sensor Interface (CSI)&lt;/P&gt;&lt;P&gt;configurations. Please also refer to attached Linux Manual with drivers description.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Apr 2017 11:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Camera-driver-porting/m-p/607725#M91664</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-13T11:33:37Z</dc:date>
    </item>
  </channel>
</rss>