<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Stereo audio in using i.MX6UL and Android Things in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Stereo-audio-in-using-i-MX6UL-and-Android-Things/m-p/607606#M91624</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We would like to implement an audio processing library on Android Things. For improved performance we want to use two microphones / audio inputs.&lt;/P&gt;&lt;P&gt;The two official Android Things development boards both feature the SGTL5000, which has stereo line in.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Pico i.MX6UL (which I was trying out already) unfortunately does not have the line in wired to a physical jack. The Android Things framework also does not seem to recognize the line in input: there is only a single input device when querying AudioDeviceInfo.&lt;/P&gt;&lt;P&gt;Is it possible to modify the Android Things system image to expose the line in as inputs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Argon does feature a separate jack line in. Can someone confirm that the line in jack supports stereo audio? This is not entirely clear from the datasheet.&lt;/P&gt;&lt;P&gt;Is it also possible to access the line in with the Android Things framework?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Koenraad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Feb 2017 15:49:20 GMT</pubDate>
    <dc:creator>koenraadverheyd</dc:creator>
    <dc:date>2017-02-28T15:49:20Z</dc:date>
    <item>
      <title>Stereo audio in using i.MX6UL and Android Things</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stereo-audio-in-using-i-MX6UL-and-Android-Things/m-p/607606#M91624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We would like to implement an audio processing library on Android Things. For improved performance we want to use two microphones / audio inputs.&lt;/P&gt;&lt;P&gt;The two official Android Things development boards both feature the SGTL5000, which has stereo line in.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Pico i.MX6UL (which I was trying out already) unfortunately does not have the line in wired to a physical jack. The Android Things framework also does not seem to recognize the line in input: there is only a single input device when querying AudioDeviceInfo.&lt;/P&gt;&lt;P&gt;Is it possible to modify the Android Things system image to expose the line in as inputs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Argon does feature a separate jack line in. Can someone confirm that the line in jack supports stereo audio? This is not entirely clear from the datasheet.&lt;/P&gt;&lt;P&gt;Is it also possible to access the line in with the Android Things framework?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Koenraad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 15:49:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stereo-audio-in-using-i-MX6UL-and-Android-Things/m-p/607606#M91624</guid>
      <dc:creator>koenraadverheyd</dc:creator>
      <dc:date>2017-02-28T15:49:20Z</dc:date>
    </item>
    <item>
      <title>Re: Stereo audio in using i.MX6UL and Android Things</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stereo-audio-in-using-i-MX6UL-and-Android-Things/m-p/607607#M91625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to modify the Android Things system image to expose the line in as inputs?. ANSWER. No, &lt;/P&gt;&lt;P style="margin-top: 0pt; margin-bottom: 0pt;"&gt;&lt;SPAN style="color: black;"&gt;Google will host and update the image &lt;/SPAN&gt;&lt;SPAN style="color: black; text-decoration: underline;"&gt;of the board that has been tested and approved,&amp;nbsp; developers only can use the USER-SPACE drivers,&amp;nbsp; provided by Google Services.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-top: 0pt; margin-bottom: 0pt;"&gt;&lt;/P&gt;&lt;P&gt;Can someone confirm that the line in jack supports stereo audio? This is not entirely clear from the datasheet.&lt;/P&gt;&lt;P&gt;Is it also possible to access the line in with the Android Things framework?&lt;/P&gt;&lt;P&gt;ANSWER.&amp;nbsp; It is better to ask ARGON regarding their HW, but based on what it is in the Web Page and in the User Manual, I would said it is possible and Android Things should have the support to handle the Line In using the Audio Service in the user space driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day sir!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Mar 2017 14:17:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stereo-audio-in-using-i-MX6UL-and-Android-Things/m-p/607607#M91625</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2017-03-01T14:17:53Z</dc:date>
    </item>
  </channel>
</rss>