<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPanic write on imx6 NAND driver</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Panic-write-on-imx6-NAND-driver/m-p/607526#M91600</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the imx6dl controller with BSP Kernel 3.10.53 and looking for a _panic_write methode,because I have to write as fast as possible when the power get lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any patches available that implement this feature ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;Wolfgang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Nov 2016 11:25:05 GMT</pubDate>
    <dc:creator>wolnet</dc:creator>
    <dc:date>2016-11-21T11:25:05Z</dc:date>
    <item>
      <title>Panic write on imx6 NAND driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Panic-write-on-imx6-NAND-driver/m-p/607526#M91600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the imx6dl controller with BSP Kernel 3.10.53 and looking for a _panic_write methode,because I have to write as fast as possible when the power get lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any patches available that implement this feature ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;Wolfgang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 11:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Panic-write-on-imx6-NAND-driver/m-p/607526#M91600</guid>
      <dc:creator>wolnet</dc:creator>
      <dc:date>2016-11-21T11:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: Panic write on imx6 NAND driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Panic-write-on-imx6-NAND-driver/m-p/607527#M91601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wolfgang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of patches, seems one can write custom driver&lt;/P&gt;&lt;P&gt;catching power loss, use for example signal on Sabre board spf-27392 p.18&lt;/P&gt;&lt;P&gt;MAX8903C&amp;nbsp; DOC output (DC UndervoltageThreshold) connected to i.MX6 EIM_CS1 or pmic :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/390440"&gt;Power fail interrupts&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 01:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Panic-write-on-imx6-NAND-driver/m-p/607527#M91601</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-11-22T01:00:45Z</dc:date>
    </item>
    <item>
      <title>Re: Panic write on imx6 NAND driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Panic-write-on-imx6-NAND-driver/m-p/607528#M91602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for the link,&lt;/P&gt;&lt;P&gt;but the information in there is only a description how to get the information that a powerfail occured.&lt;/P&gt;&lt;P&gt;This is what my target already does.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case I disable the display backlight and other things.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One of this things is to save some data to the nand flash with the function mtd_panic_write()&lt;/P&gt;&lt;P&gt;I implemented this function in Kernel 3.0.43 on my own, but this changes doesn't work on Kernel 3.10.53.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible that the Kernel configuration changes this behavior ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So what I am looking for is a implementation of _panic_write() function in gpmi_nand.c for the imx6dl controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or is there any reason why this is implemented for imx23 and imx28, ... but not for imx6 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 08:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Panic-write-on-imx6-NAND-driver/m-p/607528#M91602</guid>
      <dc:creator>wolnet</dc:creator>
      <dc:date>2016-11-22T08:16:49Z</dc:date>
    </item>
  </channel>
</rss>