<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: VDDHIGH/VSNVS diode voltage drop with MMPF0100 on startup in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-VSNVS-diode-voltage-drop-with-MMPF0100-on-startup/m-p/607274#M91534</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the same recommendation apply when using the i.MX6 Quad and Solo versions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U9 is not needed, but it is recommended for robust designs, VDDHIGH_IN in some cases may require much more current than VGEN5 can supply, so the optional LDO can supply both VDDHIGH_IN and VDD_SNVS_IN loads to meet the additional current requirements.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jan 2017 19:06:53 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2017-01-17T19:06:53Z</dc:date>
    <item>
      <title>VDDHIGH/VSNVS diode voltage drop with MMPF0100 on startup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-VSNVS-diode-voltage-drop-with-MMPF0100-on-startup/m-p/607271#M91531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;like described in the i.MX6 Datsheet Rev.4 07/2015 on page 32:&lt;/P&gt;&lt;P&gt;"VDD_SNVS_IN supply must be turned ON before any other power supply. It may be connected &lt;BR /&gt;(shorted) with VDD_HIGH_IN supply."&lt;/P&gt;&lt;P&gt;I connected&amp;nbsp;&lt;SPAN&gt;VDD_SNVS_IN and VDD_HIGH_IN at the i.MX6. Those rails are powered from the VGEN5 (+3V0_VDDHIGH) by the PMIC MMPF0100NPAZES with custom fuses. It's set to be powered first after power on.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Unfortunately I get a strange behaviour on the&amp;nbsp;+3V0_VDDHIGH rail (which is connected to the&amp;nbsp;VDD_SNVS_IN and&amp;nbsp;VDD_HIGH_IN of the i.MX6). It looks like there is a diode voltage drop on the +3V0_VDDHIGH rail (2,6V instead of 3,0V) until the second rail +1V375_VDDARM gets powered by the PMIC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could this be a problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much in advance!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2017 07:55:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-VSNVS-diode-voltage-drop-with-MMPF0100-on-startup/m-p/607271#M91531</guid>
      <dc:creator>electricar</dc:creator>
      <dc:date>2017-01-11T07:55:40Z</dc:date>
    </item>
    <item>
      <title>Re: VDDHIGH/VSNVS diode voltage drop with MMPF0100 on startup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-VSNVS-diode-voltage-drop-with-MMPF0100-on-startup/m-p/607272#M91532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This should not cause any problem, but since you are using VGEN5 to supply VDD_SNVS_IN and VDD_HIGH_IN, I want to make some extra recommendations:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In case that you are connecting VDDSNVS, a Diode (D10 in the image below) is required to correct a problem on a small number of i.MX6 DualLite parts in which VDDSNVS does not come up when VDDHIGH_IN is applied.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11108i946EE7319AAA0F00/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VDDHIGH was placed on VGEN5 early in the design as a compromise solution for a board designed primarily for software development. Validation of the i.MX6 processor has shown that operations at elevated temperatures may cause VDDHIGH_IN to require much more current than VGEN5 can supply.&lt;/P&gt;&lt;P&gt;It is recommended for robust designs potentially operating at more extreme temperatures for VDDHIGH to be supplied from a power rail that can supply 250 mA or more.&lt;/P&gt;&lt;P&gt;This allows for datasheet maximum of 125 mA for internal VDDHIGH_IN loads plus 125 mA for external PHY IO loads.&lt;/P&gt;&lt;P&gt;The optional LDO U9 shown on this page could be reconfigured to supply both VDDHIGH_IN and VDD_SNVS_IN loads to meet the additional current requirements:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11203i25010C13C22C3F81/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more details I recommend you to take a look at the attached schematic.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 22:22:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-VSNVS-diode-voltage-drop-with-MMPF0100-on-startup/m-p/607272#M91532</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2017-01-13T22:22:33Z</dc:date>
    </item>
    <item>
      <title>Re: VDDHIGH/VSNVS diode voltage drop with MMPF0100 on startup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-VSNVS-diode-voltage-drop-with-MMPF0100-on-startup/m-p/607273#M91533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jose,&lt;/P&gt;&lt;P&gt;thank you very much for your answer. We are using the i.MX6 Quad and Solo, not the DualLite.&lt;/P&gt;&lt;P&gt;Is the high current consumption on VDDHIGH a problem on the Quad version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also in the schematic this info is written near the LDO U9:&lt;/P&gt;&lt;P&gt;"U9 is no longer required for PF0100 VSNVS issue, but may be desired for NVCC_PLL_VOUT"&lt;/P&gt;&lt;P&gt;So is this still a problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 14:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-VSNVS-diode-voltage-drop-with-MMPF0100-on-startup/m-p/607273#M91533</guid>
      <dc:creator>electricar</dc:creator>
      <dc:date>2017-01-17T14:59:54Z</dc:date>
    </item>
    <item>
      <title>Re: VDDHIGH/VSNVS diode voltage drop with MMPF0100 on startup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-VSNVS-diode-voltage-drop-with-MMPF0100-on-startup/m-p/607274#M91534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the same recommendation apply when using the i.MX6 Quad and Solo versions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U9 is not needed, but it is recommended for robust designs, VDDHIGH_IN in some cases may require much more current than VGEN5 can supply, so the optional LDO can supply both VDDHIGH_IN and VDD_SNVS_IN loads to meet the additional current requirements.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 19:06:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-VSNVS-diode-voltage-drop-with-MMPF0100-on-startup/m-p/607274#M91534</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2017-01-17T19:06:53Z</dc:date>
    </item>
  </channel>
</rss>