<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6Q SabreAuto h264 decoder not decoding to full range colors in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SabreAuto-h264-decoder-not-decoding-to-full-range-colors/m-p/607192#M91518</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have issue with one of h264 stream. This is test stream to check color displayed on the LCD screen,&lt;BR /&gt;In one of the screens. It has 16 bars representing 16 shades of gray. Starting from 0,16,32 ....... 240,255.&lt;/P&gt;&lt;P&gt;Issue we are facing is that &lt;STRONG&gt;we are not able to visually differentiate between 0,16 and 240,255 shades of gray&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;We are using mxc_vpu like following command.&lt;/P&gt;&lt;P&gt;/unit_tests/mxc_vpu_test.out -D "-i video800x480x60.h264 -f2 -o 123.yuv -v h -t 0"&lt;/P&gt;&lt;P&gt;Above command line dumps video to 123.yuv file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we check the dump in pc or in board we are not able to see colors. &lt;BR /&gt;There is no difference in 0,16 and 240, 255 (towards white)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;STRONG&gt;Following is information regarding VPU&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Product Info: i.MX6Q/D/S&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;VPU firmware version: 2.1.9_r36350&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;VPU library version: 5.4.12&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Format: STD_AVC&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2016 05:00:00 GMT</pubDate>
    <dc:creator>ashutoshsrivast</dc:creator>
    <dc:date>2016-12-14T05:00:00Z</dc:date>
    <item>
      <title>IMX6Q SabreAuto h264 decoder not decoding to full range colors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SabreAuto-h264-decoder-not-decoding-to-full-range-colors/m-p/607192#M91518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have issue with one of h264 stream. This is test stream to check color displayed on the LCD screen,&lt;BR /&gt;In one of the screens. It has 16 bars representing 16 shades of gray. Starting from 0,16,32 ....... 240,255.&lt;/P&gt;&lt;P&gt;Issue we are facing is that &lt;STRONG&gt;we are not able to visually differentiate between 0,16 and 240,255 shades of gray&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;We are using mxc_vpu like following command.&lt;/P&gt;&lt;P&gt;/unit_tests/mxc_vpu_test.out -D "-i video800x480x60.h264 -f2 -o 123.yuv -v h -t 0"&lt;/P&gt;&lt;P&gt;Above command line dumps video to 123.yuv file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we check the dump in pc or in board we are not able to see colors. &lt;BR /&gt;There is no difference in 0,16 and 240, 255 (towards white)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;STRONG&gt;Following is information regarding VPU&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Product Info: i.MX6Q/D/S&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;VPU firmware version: 2.1.9_r36350&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;VPU library version: 5.4.12&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Format: STD_AVC&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 05:00:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SabreAuto-h264-decoder-not-decoding-to-full-range-colors/m-p/607192#M91518</guid>
      <dc:creator>ashutoshsrivast</dc:creator>
      <dc:date>2016-12-14T05:00:00Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q SabreAuto h264 decoder not decoding to full range colors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SabreAuto-h264-decoder-not-decoding-to-full-range-colors/m-p/607193#M91519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;do you mind uploading your h264 file, let me reproduce it on my mx6q board&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Dec 2016 06:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SabreAuto-h264-decoder-not-decoding-to-full-range-colors/m-p/607193#M91519</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2016-12-27T06:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q SabreAuto h264 decoder not decoding to full range colors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SabreAuto-h264-decoder-not-decoding-to-full-range-colors/m-p/607194#M91520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ashutosh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you fix the issue? As I am also facing same issue, it would be helpful if you could give some inputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vikash&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2018 05:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SabreAuto-h264-decoder-not-decoding-to-full-range-colors/m-p/607194#M91520</guid>
      <dc:creator>vikaspatil</dc:creator>
      <dc:date>2018-01-09T05:31:33Z</dc:date>
    </item>
  </channel>
</rss>