<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: watchdog versus reboot command - hangs sometimes</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/watchdog-versus-reboot-command-hangs-sometimes/m-p/607191#M91517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manoel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try suggestions on link for similar issue&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/321274"&gt;mx6q reboot problem&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and check with oscilloscope reset PMIC, on SabreSD schematic this is&lt;/P&gt;&lt;P&gt;spf-27392 p.19 signal pwron, generated from wdog on p.21&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Schematics (1)&lt;BR /&gt;i.MX6_SABRE_SDP_DESIGNFILES&lt;BR /&gt;&lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-platform-for-smart-devices-based-on-the-i.mx-6-series:RDIMX6SABREPLAT?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-platform-for-smart-devices-based-on-the-i.mx-6-series:RDIMX6SABREPLAT?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 20 Nov 2016 23:43:52 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-11-20T23:43:52Z</dc:date>
    <item>
      <title>watchdog versus reboot command - hangs sometimes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/watchdog-versus-reboot-command-hangs-sometimes/m-p/607189#M91515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I have a question. My device is running android 4.3 based in IMX6Q and created a script that test the boot process. Basically, after the zygote is ready, 10 seconds later I send a reboot command via shell.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;The device reboots fine for something around 10 boots. After that I see that u-boot is detecting the previous boot as "watchdog" reason and then hangs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Everytime I send the reboot, command I see the following messages:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;# reboot&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;SysRq : Emergency Remount R/O&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;EXT4-fs (mmcblk0p4): re-mounted. Opts: (null)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;EXT4-fs (mmcblk0p6): re-mounted. Opts: (null)&lt;/STRONG&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Emergency Remount complete&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;EM&gt;imx2-wdt imx2-wdt.0: Device shutdown: Expect reboot!&lt;/EM&gt;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;EM&gt;Restarting system.&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the restart fails I see the boot reason as WDOG:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2009.08-00091-gb128c3c (Nov 15 2016 - 17:01:55)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6 family TO1.2 at 792 MHz&lt;BR /&gt;Thermal sensor with ratio = 185&lt;BR /&gt;Temperature: 40 C, calibration data 0x59550269&lt;BR /&gt;mx6q pll1: 792MHz&lt;BR /&gt;mx6q pll2: 528MHz&lt;BR /&gt;mx6q pll3: 480MHz&lt;BR /&gt;mx6q pll8: 50MHz&lt;BR /&gt;ipg clock : 66000000Hz&lt;BR /&gt;ipg per clock : 66000000Hz&lt;BR /&gt;uart clock : 80000000Hz&lt;BR /&gt;cspi clock : 60000000Hz&lt;BR /&gt;ahb clock : 132000000Hz&lt;BR /&gt;axi clock : 264000000Hz&lt;BR /&gt;emi_slow clock: 132000000Hz&lt;BR /&gt;ddr clock : 528000000Hz&lt;BR /&gt;usdhc1 clock : 198000000Hz&lt;BR /&gt;usdhc2 clock : 198000000Hz&lt;BR /&gt;usdhc3 clock : 198000000Hz&lt;BR /&gt;usdhc4 clock : 198000000Hz&lt;BR /&gt;nfc clock : 24000000Hz&lt;BR /&gt;Board: i.MX6Q-HORIZON: unknown-board Board: 0x63012 [&lt;STRONG&gt;WDOG&lt;/STRONG&gt;]&lt;BR /&gt;Boot Device: MMC&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 1 GB&lt;BR /&gt;MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3&lt;BR /&gt;*** Warning - bad CRC or MMC, using default environment&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Found PFUZE100! deviceid=10,revid=21&lt;BR /&gt;Net: FEC0 [PRIME]&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;kernel @ 10808000 (4752500)&lt;BR /&gt;ramdisk @ 11800000 (238673)&lt;BR /&gt;kernel cmdline:&lt;BR /&gt; use boot.img command line:&lt;BR /&gt; console=ttymxc0,115200 init=/init video=mxcfb0:dev=lcd,Newhaven-LCD,if=RGB24,bpp=32 fbmem=28M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=intrinsyc no_console_suspend=1 dmfc=3&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;BR /&gt;Initializing cgroup subsys cpu&lt;BR /&gt;Linux version 3.0.35 (mramon@nirvana-vm) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #4 SMP PREEMPT Wed Nov 16 13:50:44 PST 2016&lt;BR /&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Machine: Accriva i.MX 6 Horizon Board&lt;BR /&gt;Memory policy: ECC disabled, Data cache writealloc&lt;BR /&gt;CPU identified as i.MX6Q, silicon rev 1.2&lt;BR /&gt;PERCPU: Embedded 7 pages/cpu @c1325000 s6592 r8192 d13888 u32768&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 203520&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=lcd,Newhaven-LCD,if=RGB24,bpp=32 fbmem=28M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=intrinsyc no_console_suspend=1 dmfc=3&lt;BR /&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;BR /&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;BR /&gt;Memory: 379MB 360MB 64MB = 803MB total&lt;BR /&gt;Memory: 801972k/801972k available, 246604k reserved, 434176K highmem&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt; vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;BR /&gt; fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)&lt;BR /&gt; DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)&lt;BR /&gt; vmalloc : 0xd9800000 - 0xf2000000 ( 392 MB)&lt;BR /&gt; lowmem : 0xc0000000 - 0xd9000000 ( 400 MB)&lt;BR /&gt; pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)&lt;BR /&gt; modules : 0xbf000000 - 0xbfe00000 ( 14 MB)&lt;BR /&gt; .init : 0xc0008000 - 0xc0065000 ( 372 kB)&lt;BR /&gt; .text : 0xc0065000 - 0xc08fc39c (8797 kB)&lt;BR /&gt; .data : 0xc08fe000 - 0xc0993688 ( 598 kB)&lt;BR /&gt; .bss : 0xc09936ac - 0xc0b1b608 (1568 kB)&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt;NR_IRQS:624&lt;BR /&gt;MXC GPIO hardware&lt;BR /&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms&lt;BR /&gt;arm_max_freq=800MHz&lt;BR /&gt;MXC_Early serial console at MMIO 0x2020000 (options '115200')&lt;BR /&gt;bootconsole [ttymxc0] enabled&lt;BR /&gt;Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 512&lt;BR /&gt;Initializing cgroup subsys debug&lt;BR /&gt;Initializing cgroup subsys cpuacct&lt;BR /&gt;Initializing cgroup subsys freezer&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available&lt;BR /&gt;CPU1: Booted secondary processor&lt;BR /&gt;Brought up 2 CPUs&lt;BR /&gt;SMP: Total of 2 processors activated (3162.11 BogoMIPS).&lt;BR /&gt;print_constraints: dummy:&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;print_constraints: vddpu: 725 &amp;lt;--&amp;gt; 1300 mV at 700 mV fast normal&lt;BR /&gt;print_constraints: vddcore: 725 &amp;lt;--&amp;gt; 1300 mV at 1150 mV fast normal&lt;BR /&gt;print_constraints: vddsoc: 725 &amp;lt;--&amp;gt; 1300 mV at 1200 mV fast normal&lt;BR /&gt;print_constraints: vdd2p5: 2000 &amp;lt;--&amp;gt; 2775 mV at 2400 mV fast normal&lt;BR /&gt;print_constraints: vdd1p1: 800 &amp;lt;--&amp;gt; 1400 mV at 1100 mV fast normal&lt;BR /&gt;print_constraints: vdd3p0: 2625 &amp;lt;--&amp;gt; 3400 mV at 3000 mV fast normal&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Reboot Reason: [WDOG]&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;Board: UARTs Initialized.&lt;/P&gt;&lt;P&gt;ram_console: got buffer at 3ff00000, size 100000&lt;BR /&gt;ram_console: found existing buffer, size 20220, start 20220&lt;BR /&gt;console [ram-1] enabled&lt;BR /&gt;Board: LCD init ok&lt;BR /&gt;Board: jadak_data enabled&lt;BR /&gt;Booting device : MMC&lt;BR /&gt;user buttons defined: ret = 0&lt;BR /&gt;------------------&lt;BR /&gt; Wifi/BT power on&lt;BR /&gt;------------------&lt;BR /&gt;Board: Analytic Camera initialized.&lt;BR /&gt;Board: Analytic POST Enabled&lt;/P&gt;&lt;P&gt;Board: 3.3VA Disabled&lt;/P&gt;&lt;P&gt;Board: Analytic CPU Disabled&lt;/P&gt;&lt;P&gt;Board: Analytic Boot init ok&lt;BR /&gt;Board: ft5x0x_ts_reset&lt;BR /&gt;Board: ft5x0x_ts_init ok&lt;BR /&gt;Board: SPARX-Integrated PCB defined.&lt;BR /&gt;Board: End of Board Init.&lt;/P&gt;&lt;P&gt;hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.&lt;BR /&gt;hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.&lt;BR /&gt;hw-breakpoint: maximum watchpoint size is 4 bytes.&lt;BR /&gt;L310 cache controller enabled&lt;BR /&gt;l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B&lt;BR /&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;BR /&gt;mxs-dma mxs-dma-apbh: initialized&lt;BR /&gt;print_constraints: vmmc: 3300 mV&lt;BR /&gt;vgaarb: loaded&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;Freescale USB OTG Driver loaded, $Revision: 1.55 $&lt;BR /&gt;mc_pfuze 1-0008: ID: 0,Full lay: 2 ,Metal lay: 1&lt;BR /&gt;mc_pfuze 1-0008: FAB: 0 ,FIN: 0&lt;BR /&gt;PFUZE: SW4 is ON&lt;BR /&gt;print_constraints: PFUZE100_SW1A: 300 &amp;lt;--&amp;gt; 1875 mV at 1300 mV&lt;BR /&gt;print_constraints: PFUZE100_SW1B: 300 &amp;lt;--&amp;gt; 1875 mV at 300 mV&lt;BR /&gt;print_constraints: PFUZE100_SW1C: 300 &amp;lt;--&amp;gt; 1875 mV at 1300 mV&lt;BR /&gt;print_constraints: PFUZE100_SW2: 3250 &amp;lt;--&amp;gt; 3300 mV at 3300 mV&lt;BR /&gt;print_constraints: PFUZE100_SW3A: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_SW3B: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_SW4: 3200 &amp;lt;--&amp;gt; 3300 mV at 3300 mV&lt;BR /&gt;print_constraints: PFUZE100_SWBST: at 5000 mV&lt;BR /&gt;print_constraints: PFUZE100_VSNVS: 3000 mV&lt;BR /&gt;print_constraints: PFUZE100_VREFDDR: at 750 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN1: 800 &amp;lt;--&amp;gt; 1550 mV at 800 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN2: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN3: 3000 &amp;lt;--&amp;gt; 3300 mV at 3300 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN4: 2800 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN5: 2800 &amp;lt;--&amp;gt; 3000 mV at 2800 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN6: 3100 &amp;lt;--&amp;gt; 3300 mV at 3300 mV&lt;BR /&gt;MANOEL ipu_proble()&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: IPU DMFC ONLY-DP HIGH RESOLUTION: 5B(0~3), 5F(4~7)&lt;BR /&gt;MANOEL ipu_proble()&lt;BR /&gt;imx-ipuv3 imx-ipuv3.1: IPU DMFC ONLY-DP HIGH RESOLUTION: 5B(0~3), 5F(4~7)&lt;BR /&gt;Advanced Linux Sound Architecture Driver Version 1.0.24.&lt;BR /&gt;Bluetooth: Core ver 2.16&lt;BR /&gt;NET: Registered protocol family 31&lt;BR /&gt;Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;Bluetooth: HCI socket layer initialized&lt;BR /&gt;Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;Bluetooth: SCO socket layer initialized&lt;BR /&gt;i2c-core: driver [max17135] using legacy suspend method&lt;BR /&gt;i2c-core: driver [max17135] using legacy resume method&lt;BR /&gt;Switching to clocksource mxc_timer1&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;IP route cache hash table entries: 16384 (order: 4, 65536 bytes)&lt;BR /&gt;TCP established hash table entries: 65536 (order: 7, 524288 bytes)&lt;BR /&gt;TCP bind hash table entries: 65536 (order: 7, 786432 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 65536 bind 65536)&lt;BR /&gt;TCP reno registered&lt;BR /&gt;UDP hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered named UNIX socket transport module.&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;PCI: CLS 0 bytes, default 32&lt;BR /&gt;Unpacking initramfs...&lt;BR /&gt;Freeing initrd memory: 232K&lt;BR /&gt;PMU: registered new PMU device of type 0&lt;BR /&gt;Static Power Management for Freescale i.MX6&lt;BR /&gt;wait mode is enabled for i.MX6&lt;BR /&gt;cpaddr = d9880000 suspend_iram_base=d98ec000&lt;BR /&gt;PM driver module loaded&lt;BR /&gt;IMX usb wakeup probe&lt;BR /&gt;the wakeup pdata is 0xd46fd8e0&lt;BR /&gt;add wake up source irq 75&lt;BR /&gt;cpu regulator mode:ldo_bypass&lt;BR /&gt;_regulator_get: get() with no identifier&lt;BR /&gt;mx6_cpu_regulator_init: failed to get pu regulator&lt;BR /&gt;i.MXC CPU frequency driver&lt;BR /&gt;highmem bounce pool size: 64 pages&lt;BR /&gt;ashmem: initialized&lt;BR /&gt;NTFS driver 2.1.30 [Flags: R/O].&lt;BR /&gt;JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;fuse init (API version 7.16)&lt;BR /&gt;msgmni has been set to 718&lt;BR /&gt;NET: Registered protocol family 38&lt;BR /&gt;cryptodev: driver loaded.&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;MIPI DSI driver module loaded&lt;BR /&gt;mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver lcd&lt;BR /&gt;&lt;STRONG&gt;lcdif_init: 1&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init channel = 9&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init channel 1&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init channel 2&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init channel 3&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init channel 23&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init channel 23.1&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init channel 23.2&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init channel 28&lt;/STRONG&gt;&lt;BR /&gt;▒&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My first question is, do you guys have any idea why sometimes the reboot is triggering the watchdog ? And why the boot fails ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Nov 2016 23:44:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/watchdog-versus-reboot-command-hangs-sometimes/m-p/607189#M91515</guid>
      <dc:creator>manoelramon</dc:creator>
      <dc:date>2016-11-18T23:44:50Z</dc:date>
    </item>
    <item>
      <title>Re: watchdog versus reboot command - hangs sometimes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/watchdog-versus-reboot-command-hangs-sometimes/m-p/607190#M91516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just to clarify. I am not sure why but after some reboots the reboot is being categorized as WDOG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why ???&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then my displays keeps off, my driver is not loaded and ipu init channel buffer is not called.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 19 Nov 2016 04:39:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/watchdog-versus-reboot-command-hangs-sometimes/m-p/607190#M91516</guid>
      <dc:creator>manoelramon</dc:creator>
      <dc:date>2016-11-19T04:39:43Z</dc:date>
    </item>
    <item>
      <title>Re: watchdog versus reboot command - hangs sometimes</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/watchdog-versus-reboot-command-hangs-sometimes/m-p/607191#M91517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manoel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try suggestions on link for similar issue&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/321274"&gt;mx6q reboot problem&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and check with oscilloscope reset PMIC, on SabreSD schematic this is&lt;/P&gt;&lt;P&gt;spf-27392 p.19 signal pwron, generated from wdog on p.21&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Schematics (1)&lt;BR /&gt;i.MX6_SABRE_SDP_DESIGNFILES&lt;BR /&gt;&lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-platform-for-smart-devices-based-on-the-i.mx-6-series:RDIMX6SABREPLAT?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-platform-for-smart-devices-based-on-the-i.mx-6-series:RDIMX6SABREPLAT?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Nov 2016 23:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/watchdog-versus-reboot-command-hangs-sometimes/m-p/607191#M91517</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-11-20T23:43:52Z</dc:date>
    </item>
  </channel>
</rss>