<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: VPU and sub-frame synchronisation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VPU-and-sub-frame-synchronisation/m-p/607149#M91511</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stéphane&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems there is some misunderstanding regarding "sub-frame sync" - it is done&lt;/P&gt;&lt;P&gt;on system level, that is linux or software does not affect it, as it is always enabled.&lt;/P&gt;&lt;P&gt;From RM:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9344iE6C50F6D1E48A941/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also please check attached Linux Manual Chapter 18&lt;BR /&gt;Video Processing Unit (VPU) Driver describing linux vpu driver.&lt;/P&gt;&lt;P&gt;I am not aware of any vpu latency "benchmark reference".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Nov 2016 01:05:53 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-11-22T01:05:53Z</dc:date>
    <item>
      <title>VPU and sub-frame synchronisation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VPU-and-sub-frame-synchronisation/m-p/607146#M91508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd like to know if the sub-frame synchronisation is enabled in the IMX6QPlus family.&lt;/P&gt;&lt;P&gt;In particular, the IMX6QPlus reference manual says yes BUT the IMX Linux API says no !!&lt;/P&gt;&lt;P&gt;Do you if sub-frame sync is enabled ?&lt;/P&gt;&lt;P&gt;Also, is there some info about the en-to-end latency for video transmission&lt;/P&gt;&lt;P&gt;between two IMX, with wifi dongles (over USB ?)&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Nov 2016 09:48:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VPU-and-sub-frame-synchronisation/m-p/607146#M91508</guid>
      <dc:creator>stéphanemancini</dc:creator>
      <dc:date>2016-11-18T09:48:42Z</dc:date>
    </item>
    <item>
      <title>Re: VPU and sub-frame synchronisation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VPU-and-sub-frame-synchronisation/m-p/607147#M91509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stéphane&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linux may implement less functionality than hardware has, please use&lt;/P&gt;&lt;P&gt;attached Linux Manual describing drivers implemented in NXP BSPs.&lt;/P&gt;&lt;P&gt;Typical latency is about 3 frame and depends on video,&amp;nbsp; also one can check&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/thread/323418"&gt;https://community.freescale.com/thread/323418&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 05:46:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VPU-and-sub-frame-synchronisation/m-p/607147#M91509</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-11-21T05:46:42Z</dc:date>
    </item>
    <item>
      <title>Re: VPU and sub-frame synchronisation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VPU-and-sub-frame-synchronisation/m-p/607148#M91510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;I read this file and also&lt;/P&gt;&lt;P&gt;IMX6DQPRM.pdf&lt;/P&gt;&lt;P&gt;i.MX_VPU_Application_Programming_Interface_Linux_Reference_Manual.pdf&lt;/P&gt;&lt;P&gt;Please, do you know if SUB-FRAME sync is enabled in the Linux driver ?&lt;/P&gt;&lt;P&gt;Is there a way to use this hardware feature ?&lt;/P&gt;&lt;P&gt;It should theoretically reduce the end-to-end latency by 2 frames (one at compression one at de-compression).&lt;/P&gt;&lt;P&gt;How is it possible to use it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, &lt;A href="https://community.nxp.com/thread/320583"&gt;i.MX6 Video Latency&lt;/A&gt;&amp;nbsp; reports a end-to-end latency of 59ms thanks to the appropriate driver.&lt;/P&gt;&lt;P&gt;Unfortunately the frame rate and resolution informations are missing.&lt;/P&gt;&lt;P&gt;The thread you provide is about imx53 and the reported delay is 200 to 300 ms (nothing relates).&lt;/P&gt;&lt;P&gt;Also, some guys &lt;A href="https://community.nxp.com/message/498952"&gt;https://community.nxp.com/message/498952&lt;/A&gt;&amp;nbsp; reports 'zero delay' thanks to i&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;ntra refresh frames but they do not provide numbers.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Does NXP has a benchmark reference ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Stéphane&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 10:52:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VPU-and-sub-frame-synchronisation/m-p/607148#M91510</guid>
      <dc:creator>stéphanemancini</dc:creator>
      <dc:date>2016-11-21T10:52:26Z</dc:date>
    </item>
    <item>
      <title>Re: VPU and sub-frame synchronisation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VPU-and-sub-frame-synchronisation/m-p/607149#M91511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stéphane&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems there is some misunderstanding regarding "sub-frame sync" - it is done&lt;/P&gt;&lt;P&gt;on system level, that is linux or software does not affect it, as it is always enabled.&lt;/P&gt;&lt;P&gt;From RM:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9344iE6C50F6D1E48A941/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also please check attached Linux Manual Chapter 18&lt;BR /&gt;Video Processing Unit (VPU) Driver describing linux vpu driver.&lt;/P&gt;&lt;P&gt;I am not aware of any vpu latency "benchmark reference".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 01:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VPU-and-sub-frame-synchronisation/m-p/607149#M91511</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-11-22T01:05:53Z</dc:date>
    </item>
  </channel>
</rss>