<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB supplied while i.MX6 is off in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-supplied-while-i-MX6-is-off/m-p/606803#M91429</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, i.MX6DQ Datasheet sect.4.2.1 Power-Up Sequence describes:&lt;/P&gt;&lt;P&gt;USB_OTG_VBUS and USB_H1_VBUS are not part of the power supply&lt;BR /&gt;sequence and can be powered at any time.&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Feb 2017 00:48:56 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-02-07T00:48:56Z</dc:date>
    <item>
      <title>USB supplied while i.MX6 is off</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-supplied-while-i-MX6-is-off/m-p/606802#M91428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;am I getting this right, that it's not a problem when the USB ports of the i.MX6 are powered from another device while the i.MX6 is off (not powered)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 12:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-supplied-while-i-MX6-is-off/m-p/606802#M91428</guid>
      <dc:creator>electricar</dc:creator>
      <dc:date>2017-02-06T12:33:07Z</dc:date>
    </item>
    <item>
      <title>Re: USB supplied while i.MX6 is off</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-supplied-while-i-MX6-is-off/m-p/606803#M91429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, i.MX6DQ Datasheet sect.4.2.1 Power-Up Sequence describes:&lt;/P&gt;&lt;P&gt;USB_OTG_VBUS and USB_H1_VBUS are not part of the power supply&lt;BR /&gt;sequence and can be powered at any time.&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 00:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-supplied-while-i-MX6-is-off/m-p/606803#M91429</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-07T00:48:56Z</dc:date>
    </item>
  </channel>
</rss>