<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Adding patches to build uImage (AVB)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Adding-patches-to-build-uImage-AVB/m-p/605776#M91298</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ajay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please refer to yocto faq sect.2.2.2. Applying Patches&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.yoctoproject.org/docs/1.6.1/kernel-dev/kernel-dev.html#applying-patches" title="https://www.yoctoproject.org/docs/1.6.1/kernel-dev/kernel-dev.html#applying-patches"&gt;Yocto Project Linux Kernel Development Manual&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;H3 class=""&gt;&lt;/H3&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2016 05:11:02 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-12-14T05:11:02Z</dc:date>
    <item>
      <title>Adding patches to build uImage (AVB)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-patches-to-build-uImage-AVB/m-p/605775#M91297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I want to build a uImage for AVB. I have found the link with the required patches needed to build the uImage. But how and where should I add these patches for building the image? Should I add it in the local.conf file and if yes, how do I add it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 12:15:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-patches-to-build-uImage-AVB/m-p/605775#M91297</guid>
      <dc:creator>ajayvenkatakris</dc:creator>
      <dc:date>2016-12-13T12:15:00Z</dc:date>
    </item>
    <item>
      <title>Re: Adding patches to build uImage (AVB)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-patches-to-build-uImage-AVB/m-p/605776#M91298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ajay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please refer to yocto faq sect.2.2.2. Applying Patches&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.yoctoproject.org/docs/1.6.1/kernel-dev/kernel-dev.html#applying-patches" title="https://www.yoctoproject.org/docs/1.6.1/kernel-dev/kernel-dev.html#applying-patches"&gt;Yocto Project Linux Kernel Development Manual&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;H3 class=""&gt;&lt;/H3&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 05:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-patches-to-build-uImage-AVB/m-p/605776#M91298</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-14T05:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: Adding patches to build uImage (AVB)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-patches-to-build-uImage-AVB/m-p/605777#M91299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; There are many bbappend files available. I am building an fsl-image-gui for imx6dl sabre auto board. At exactly which bbappend file should I add the patch files?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 17:18:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-patches-to-build-uImage-AVB/m-p/605777#M91299</guid>
      <dc:creator>ajayvenkatakris</dc:creator>
      <dc:date>2016-12-14T17:18:59Z</dc:date>
    </item>
  </channel>
</rss>