<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: PHP 7.1.0 Yocto Build Error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605514#M91268</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As do_install failed, is there any error/log message?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Feb 2017 09:37:11 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2017-02-08T09:37:11Z</dc:date>
    <item>
      <title>PHP 7.1.0 Yocto Build Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605513#M91267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I m using yocto to generate image &amp;nbsp;and I want to include php 7.1.0 to my image but I got task error&amp;nbsp;&lt;/P&gt;&lt;P&gt;Task (/home/mustafa/fsl-community-bsp/sources/meta-openembedded/meta-oe/recipes-devtools/php/php_7.1.0.bb:do_install) failed with exit code '1'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and when go &amp;nbsp;to the /build / deploy/rpm &amp;nbsp;/ armv7at2hf_neon / directory I can see the php 7.1.0 rpm packages ,&lt;/P&gt;&lt;P&gt;Which I need to use these packages at &amp;nbsp;my wandboard directory and my wandboard image &amp;nbsp;. Is there any recommandation about this ?&lt;/P&gt;&lt;P&gt;Or should I have to do it different way ? Is there any solution ___???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 19:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605513#M91267</guid>
      <dc:creator>mustafabakircio</dc:creator>
      <dc:date>2017-02-06T19:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: PHP 7.1.0 Yocto Build Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605514#M91268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As do_install failed, is there any error/log message?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2017 09:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605514#M91268</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-02-08T09:37:11Z</dc:date>
    </item>
    <item>
      <title>Re: PHP 7.1.0 Yocto Build Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605515#M91269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jimmychan ;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: php-7.1.0-r0 do_install: Function failed: do_install (log file is located at /home/mustafa/fsl-community-bsp/build/tmp/work/armv7at2hf-neon-fslc-linux-gnueabi/php/7.1.0-r0/temp/log.do_install.656)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/mustafa/fsl-community-bsp/build/tmp/work/armv7at2hf-neon-fslc-linux-gnueabi/php/7.1.0-r0/temp/log.do_install.656&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;| ERROR: One of /home/mustafa/.pearrc or /home/mustafa/fsl-community-bsp/build/tmp/work/armv7at2hf-neon-fslc-linux-gnueabi/php/7.1.0-r0/recipe-sysroot-native/usr/bin/../../etc//pear.conf is corrupt, please remove them and try againInstalling PHP FPM man page: /home/mustafa/fsl-community-bsp/build/tmp/work/armv7at2hf-neon-fslc-linux-gnueabi/php/7.1.0-r0/image/usr/share/man/man8/&lt;BR /&gt;| Installing PHP FPM status page: /home/mustafa/fsl-community-bsp/build/tmp/work/armv7at2hf-neon-fslc-linux-gnueabi/php/7.1.0-r0/image/usr/share/fpm/&lt;BR /&gt;| Installing header files: /home/mustafa/fsl-community-bsp/build/tmp/work/armv7at2hf-neon-fslc-linux-gnueabi/php/7.1.0-r0/image/usr/include/php/&lt;BR /&gt;| sed: can't read /home/mustafa/fsl-community-bsp/build/tmp/work/armv7at2hf-neon-fslc-linux-gnueabi/php/7.1.0-r0/image//etc/pear.conf: No such file or directory&lt;BR /&gt;| WARNING: exit code 2 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_install (log file is located at /home/mustafa/fsl-community-bsp/build/tmp/work/armv7at2hf-neon-fslc-linux-gnueabi/php/7.1.0-r0/temp/log.do_install.656)&lt;BR /&gt;ERROR: Task (/home/mustafa/fsl-community-bsp/sources/meta-openembedded/meta-oe/recipes-devtools/php/php_7.1.0.bb:do_install) failed with exit code '1'&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2017 10:49:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605515#M91269</guid>
      <dc:creator>mustafabakircio</dc:creator>
      <dc:date>2017-02-08T10:49:46Z</dc:date>
    </item>
    <item>
      <title>Re: PHP 7.1.0 Yocto Build Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605516#M91270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;seems the pear.conf is corrupt, so the error "pear.conf: No such file or directory"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Feb 2017 07:15:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605516#M91270</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-02-09T07:15:34Z</dc:date>
    </item>
    <item>
      <title>Re: PHP 7.1.0 Yocto Build Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605517#M91271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do I need to find the correct patch or is there another way you can suggest ,jimmychan ?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Feb 2017 16:12:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605517#M91271</guid>
      <dc:creator>mustafabakircio</dc:creator>
      <dc:date>2017-02-09T16:12:07Z</dc:date>
    </item>
    <item>
      <title>Re: PHP 7.1.0 Yocto Build Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605518#M91272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;maybe you can try php 7.1.1&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.linuxfromscratch.org/blfs/view/svn/general/php.html" title="http://www.linuxfromscratch.org/blfs/view/svn/general/php.html"&gt;PHP-7.1.1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2017 09:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PHP-7-1-0-Yocto-Build-Error/m-p/605518#M91272</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-02-10T09:11:54Z</dc:date>
    </item>
  </channel>
</rss>