<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6 Dual RAM Supported?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Dual-RAM-Supported/m-p/605356#M91235</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; it is possible to use the mentioned part with i.MX6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.alliancememory.com/pdf/ddr3/8GB-AS4C512M16D3L.pdf" title="http://www.alliancememory.com/pdf/ddr3/8GB-AS4C512M16D3L.pdf"&gt;http://www.alliancememory.com/pdf/ddr3/8GB-AS4C512M16D3L.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please use the &lt;A href="https://community.nxp.com/docs/DOC-94917"&gt;https://community.nxp.com/docs/DOC-94917&lt;/A&gt; to configure the memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Sep 2016 07:47:18 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-09-13T07:47:18Z</dc:date>
    <item>
      <title>i.MX6 Dual RAM Supported?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Dual-RAM-Supported/m-p/605355#M91234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about what RAM the MX6 Dual will support. I am looking to use part number:&amp;nbsp;MCIMX6D7CVT08AD.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the reference design (which uses a QuadCore MX6Q) they call out Quantity 4: DDR3L 2Gb RAM at 800MHz to reach 1GB total.&lt;/P&gt;&lt;P&gt;In the combined datasheet for the Quad and Dual it says only DDR3-1066 and LPDDR2-1066 are supported (see attached printscreen).&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm having a hard time finding non-last time buy or obsolete RAM at 533MHz/1066 Data Rate.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, with the Dual model I've chosen can I use an 800MHz module such as the one below, or is there a functional difference that only allows the MX6Q to use 800MHz/1600 data rate RAM?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Alliance Memory:&amp;nbsp;AS4C512M16D3L-12BCN&amp;nbsp;&lt;/P&gt;&lt;P&gt;If this won't work can you suggest a 1GB (8Gb) module I could use that is active (in production)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your time and help.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 14:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Dual-RAM-Supported/m-p/605355#M91234</guid>
      <dc:creator>rmstark</dc:creator>
      <dc:date>2016-09-09T14:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Dual RAM Supported?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Dual-RAM-Supported/m-p/605356#M91235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; it is possible to use the mentioned part with i.MX6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.alliancememory.com/pdf/ddr3/8GB-AS4C512M16D3L.pdf" title="http://www.alliancememory.com/pdf/ddr3/8GB-AS4C512M16D3L.pdf"&gt;http://www.alliancememory.com/pdf/ddr3/8GB-AS4C512M16D3L.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please use the &lt;A href="https://community.nxp.com/docs/DOC-94917"&gt;https://community.nxp.com/docs/DOC-94917&lt;/A&gt; to configure the memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 07:47:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Dual-RAM-Supported/m-p/605356#M91235</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-13T07:47:18Z</dc:date>
    </item>
  </channel>
</rss>