<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SIM interface iMX6UL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SIM-interface-iMX6UL/m-p/605307#M91230</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am bit confuse about SIM interface on iMX6UL.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per technical reference manual page # 2799, "The SIM module has one port&amp;nbsp;that can be used to interface with the various cards." &amp;nbsp;But block diagram shows two port, 0 &amp;amp; 1.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5210iB490D5D77A2DA590/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Referred i.MX6UL pin muxing, Found that there are four ports.&lt;/P&gt;&lt;P&gt;SIM1.Port0,&lt;/P&gt;&lt;P&gt;SIM1.Port1,&lt;/P&gt;&lt;P&gt;SIM2.Port0,&lt;/P&gt;&lt;P&gt;SIM2.Port1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will appreciate any help or clarification&amp;nbsp;for understanding above with reference if any.&lt;/P&gt;&lt;P&gt;Can you please let me know on which two SIM&amp;nbsp;ports&amp;nbsp;i can connect smart card? As datasheet shows upto 2 SIM interface support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Sep 2016 04:45:53 GMT</pubDate>
    <dc:creator>riteshpatel</dc:creator>
    <dc:date>2016-09-09T04:45:53Z</dc:date>
    <item>
      <title>SIM interface iMX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SIM-interface-iMX6UL/m-p/605307#M91230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am bit confuse about SIM interface on iMX6UL.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per technical reference manual page # 2799, "The SIM module has one port&amp;nbsp;that can be used to interface with the various cards." &amp;nbsp;But block diagram shows two port, 0 &amp;amp; 1.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5210iB490D5D77A2DA590/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Referred i.MX6UL pin muxing, Found that there are four ports.&lt;/P&gt;&lt;P&gt;SIM1.Port0,&lt;/P&gt;&lt;P&gt;SIM1.Port1,&lt;/P&gt;&lt;P&gt;SIM2.Port0,&lt;/P&gt;&lt;P&gt;SIM2.Port1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will appreciate any help or clarification&amp;nbsp;for understanding above with reference if any.&lt;/P&gt;&lt;P&gt;Can you please let me know on which two SIM&amp;nbsp;ports&amp;nbsp;i can connect smart card? As datasheet shows upto 2 SIM interface support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 04:45:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SIM-interface-iMX6UL/m-p/605307#M91230</guid>
      <dc:creator>riteshpatel</dc:creator>
      <dc:date>2016-09-09T04:45:53Z</dc:date>
    </item>
    <item>
      <title>Re: SIM interface iMX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SIM-interface-iMX6UL/m-p/605308#M91231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Each SIM module can be connected to two separate devices via Port0 and Port1, &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;however communication to two devices from a single SIM module is alternate and &lt;BR /&gt;can not provide simultaneous communication. Please refer to SIM Setup Register&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;how to configure ports.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 06:22:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SIM-interface-iMX6UL/m-p/605308#M91231</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-09T06:22:52Z</dc:date>
    </item>
  </channel>
</rss>