<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 USB connection-disconnection problem on iMX6SoloX</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-connection-disconnection-problem-on-iMX6SoloX/m-p/605093#M91179</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, everybody.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First of all a little bit of context. I have a device that has just one USB port with a micro USB connector. This port is used for serial flashing and when the device is operating normally nothing is connected to this micro USB connector except for the power supply of the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recently discovered that we need to connect an RTL-SDR&amp;nbsp;dongle to this device but we can't perform any modifications to the already existing hardware, therefore I thought that I could just provide power to this device through the USB power pins and provide the RTL-SDR dongle data trough the D+ and D- pins of that same connector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not a standard setup&amp;nbsp;because normally, the USB HOST is the one providing power to the USB device when it is connected to the HOST in an OTG configuration. &amp;nbsp;But in this scenario, it has to be the other way around and &lt;EM&gt;I don't know if this is causing the problem in the first place&lt;/EM&gt;. I assume that this is not the problem because it is transparent to both devices, &lt;STRONG&gt;or is it?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since there is no device that provides power to the host I had to hardware-hack a little bit and I have the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="hardwareHack.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12759i177E8C6C64D42EE5/image-size/large?v=v2&amp;amp;px=999" role="button" title="hardwareHack.jpg" alt="hardwareHack.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That way I can provide power to both HOST and DEVICE and also I can remove the power from the DEVICE if needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is that it doesn't matter if I power both at the same time or if I power the HOST first and then the RTL-SDR dongle once the HOST is ready, I get this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 2 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 2&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 3 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 3&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 4 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 5 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 5&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 6 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 6&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 7 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 7&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 8 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 8&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 9 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 9&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 10 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 10&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 11 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 11&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 12 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 12&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 13 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 13&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 14 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 14&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 15 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: USB disconnect, device number 15&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And it continues until reaching 127 and then it starts again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then if I SSH into the board and I run the rtl_tcp utility I get:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Found 1 device(s):&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;0: , , SN:&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Using device 0: Generic RTL2832U OEM&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;No supported tuner found&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Enabled direct sampling mode, input 1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;WARNING: Failed to set sample rate.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;WARNING: Failed to set center freq.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;listening...&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Use the device argument 'rtl_tcp=127.0.0.1:1234' in OsmoSDR (gr-&lt;/STRONG&gt;&lt;/SPAN&gt;osmosdr&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;) source&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;to receive samples in GRC and control rtl_tcp parameters (frequency, gain, ...).&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, &lt;STRONG&gt;does anybody know what is going on?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Feb 2017 16:37:15 GMT</pubDate>
    <dc:creator>m4l490n</dc:creator>
    <dc:date>2017-02-06T16:37:15Z</dc:date>
    <item>
      <title>USB connection-disconnection problem on iMX6SoloX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-connection-disconnection-problem-on-iMX6SoloX/m-p/605093#M91179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, everybody.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First of all a little bit of context. I have a device that has just one USB port with a micro USB connector. This port is used for serial flashing and when the device is operating normally nothing is connected to this micro USB connector except for the power supply of the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recently discovered that we need to connect an RTL-SDR&amp;nbsp;dongle to this device but we can't perform any modifications to the already existing hardware, therefore I thought that I could just provide power to this device through the USB power pins and provide the RTL-SDR dongle data trough the D+ and D- pins of that same connector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not a standard setup&amp;nbsp;because normally, the USB HOST is the one providing power to the USB device when it is connected to the HOST in an OTG configuration. &amp;nbsp;But in this scenario, it has to be the other way around and &lt;EM&gt;I don't know if this is causing the problem in the first place&lt;/EM&gt;. I assume that this is not the problem because it is transparent to both devices, &lt;STRONG&gt;or is it?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since there is no device that provides power to the host I had to hardware-hack a little bit and I have the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="hardwareHack.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12759i177E8C6C64D42EE5/image-size/large?v=v2&amp;amp;px=999" role="button" title="hardwareHack.jpg" alt="hardwareHack.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That way I can provide power to both HOST and DEVICE and also I can remove the power from the DEVICE if needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is that it doesn't matter if I power both at the same time or if I power the HOST first and then the RTL-SDR dongle once the HOST is ready, I get this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 2 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 2&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 3 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 3&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 4 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 5 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 5&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 6 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 6&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 7 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 7&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 8 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 8&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 9 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 9&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 10 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 10&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 11 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 11&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 12 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 12&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 13 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 13&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 14 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;usb&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt; 1-1: USB disconnect, device number 14&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: new high-speed USB device number 15 using ci_hdrc&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;usb&lt;STRONG&gt; 1-1: USB disconnect, device number 15&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And it continues until reaching 127 and then it starts again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then if I SSH into the board and I run the rtl_tcp utility I get:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Found 1 device(s):&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;0: , , SN:&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Using device 0: Generic RTL2832U OEM&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;No supported tuner found&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Enabled direct sampling mode, input 1&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;WARNING: Failed to set sample rate.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_demod_read_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;WARNING: Failed to set center freq.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;rtlsdr_write_reg failed with -4&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;listening...&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Use the device argument 'rtl_tcp=127.0.0.1:1234' in OsmoSDR (gr-&lt;/STRONG&gt;&lt;/SPAN&gt;osmosdr&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;) source&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;to receive samples in GRC and control rtl_tcp parameters (frequency, gain, ...).&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, &lt;STRONG&gt;does anybody know what is going on?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 16:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-connection-disconnection-problem-on-iMX6SoloX/m-p/605093#M91179</guid>
      <dc:creator>m4l490n</dc:creator>
      <dc:date>2017-02-06T16:37:15Z</dc:date>
    </item>
    <item>
      <title>Re: USB connection-disconnection problem on iMX6SoloX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-connection-disconnection-problem-on-iMX6SoloX/m-p/605094#M91180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can set mode is software using sect.39.3.8 Changing the Controller Operation Mode&lt;/P&gt;&lt;P&gt;attached Linux Manual, from hardware check processor USB_OTG_VBUS, USB_OTG_ID&lt;/P&gt;&lt;P&gt;(should be low in host mode).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 08:08:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-connection-disconnection-problem-on-iMX6SoloX/m-p/605094#M91180</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-07T08:08:18Z</dc:date>
    </item>
    <item>
      <title>Re: USB connection-disconnection problem on iMX6SoloX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-connection-disconnection-problem-on-iMX6SoloX/m-p/605095#M91181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks! that helped.&lt;/P&gt;&lt;P&gt;I just added &lt;STRONG&gt;dr_mode = "host";&lt;/STRONG&gt;&amp;nbsp;to my device tree and that solved the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2017 18:15:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-connection-disconnection-problem-on-iMX6SoloX/m-p/605095#M91181</guid>
      <dc:creator>m4l490n</dc:creator>
      <dc:date>2017-02-08T18:15:22Z</dc:date>
    </item>
  </channel>
</rss>