<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX7 PXP and Bayer RGB data</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-PXP-and-Bayer-RGB-data/m-p/604673#M91102</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the reference manual I have read the following about the csi interface:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Bayer data is a type of raw data from the image sensor. This byte-wide data must be&lt;BR /&gt;converted to the RGB space or YUV space by software. The data path for Bayer data is&lt;BR /&gt;from the CSI to memory".&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the csi interface can't demosaic the bayer rgb data. What about the pixel pipeline, can it convert the data&lt;/P&gt;&lt;P&gt;to rgb?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Feb 2017 13:16:50 GMT</pubDate>
    <dc:creator>fabian1993</dc:creator>
    <dc:date>2017-02-06T13:16:50Z</dc:date>
    <item>
      <title>i.MX7 PXP and Bayer RGB data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-PXP-and-Bayer-RGB-data/m-p/604673#M91102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the reference manual I have read the following about the csi interface:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Bayer data is a type of raw data from the image sensor. This byte-wide data must be&lt;BR /&gt;converted to the RGB space or YUV space by software. The data path for Bayer data is&lt;BR /&gt;from the CSI to memory".&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the csi interface can't demosaic the bayer rgb data. What about the pixel pipeline, can it convert the data&lt;/P&gt;&lt;P&gt;to rgb?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 13:16:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-PXP-and-Bayer-RGB-data/m-p/604673#M91102</guid>
      <dc:creator>fabian1993</dc:creator>
      <dc:date>2017-02-06T13:16:50Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 PXP and Bayer RGB data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-PXP-and-Bayer-RGB-data/m-p/604674#M91103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fabian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;supported PxP CSC formats are described in sect.13.7.3 Top-level architecture i.MX7D Reference Manual,&lt;/P&gt;&lt;P&gt;I am afraid raw data convertion to rgb is not supported.&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fref_manual%2FIMX7DRM.pdf" rel="nofollow" target="_blank"&gt;http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 01:02:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-PXP-and-Bayer-RGB-data/m-p/604674#M91103</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-07T01:02:26Z</dc:date>
    </item>
  </channel>
</rss>