<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Imx28 GPIO gate keeper in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Imx28-GPIO-gate-keeper/m-p/188117#M9110</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The GPIO pins will revert to input will gate keeper enabled once a valid reset is detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In your application, it is suggested to use an external pull-up or pull-down on the pin to make sure the pin for driving the fet is in a correct state out of reset.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Sep 2012 04:26:07 GMT</pubDate>
    <dc:creator>arthur_lai</dc:creator>
    <dc:date>2012-09-18T04:26:07Z</dc:date>
    <item>
      <title>Imx28 GPIO gate keeper</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx28-GPIO-gate-keeper/m-p/188116#M9109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm involved in a new imx28 hardware design .&lt;/P&gt;&lt;P&gt;I need information about status of GPIO pin when the reset is active and immediately after , when the reset is released .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reading IMX28 data sheet reference manuale , I found the following information :&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;STRONG style="font-size: 18pt; font-family: Arial;"&gt;&lt;STRONG style="font-size: 18pt; font-family: Arial;"&gt;&amp;nbsp; &lt;/STRONG&gt;&lt;/STRONG&gt;&lt;/STRONG&gt;9.2.1 Reset Configuration&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 14pt; font-family: Times New Roman;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P align="left"&gt;Out of reset (hardware/software reset), all the pins (except JTAG related) are&lt;/P&gt;&lt;P align="left"&gt;configured&lt;SPAN style="font-size: 14pt; font-family: Times New Roman;"&gt; &lt;/SPAN&gt;as GPIO inputs with gate keepers enabled.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I need to know :&lt;/P&gt;&lt;P&gt;1) When the reset pin is active (that is : RESET = LOW) are the GPIO pins input (high impedance) or the gate keeper is already enabled ?&lt;/P&gt;&lt;P&gt;2) I need information about structure of gate keeper ; gate keeper sink/source current or is high impedance&amp;nbsp; circuit ?&lt;/P&gt;&lt;P&gt;Gate keeper looks like as a weak pull up or weak pull down but it si not very clear&amp;nbsp; ! In the case that the GPIO pin&lt;/P&gt;&lt;P&gt;is connected&amp;nbsp; to drive a mosfet gate for a led activation , wihich is the logic level present on the GPIO pin when gate&lt;/P&gt;&lt;P&gt;keeper is enabled ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2012 08:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx28-GPIO-gate-keeper/m-p/188116#M9109</guid>
      <dc:creator>Fquattro</dc:creator>
      <dc:date>2012-09-10T08:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: Imx28 GPIO gate keeper</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx28-GPIO-gate-keeper/m-p/188117#M9110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The GPIO pins will revert to input will gate keeper enabled once a valid reset is detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In your application, it is suggested to use an external pull-up or pull-down on the pin to make sure the pin for driving the fet is in a correct state out of reset.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2012 04:26:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx28-GPIO-gate-keeper/m-p/188117#M9110</guid>
      <dc:creator>arthur_lai</dc:creator>
      <dc:date>2012-09-18T04:26:07Z</dc:date>
    </item>
  </channel>
</rss>