<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: show to framebuffer from IPU   in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/show-to-framebuffer-from-IPU-160/m-p/604334#M91031</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;Hi Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rotation and flip is supported by IPU, for examples one can look at&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="94961" data-objecttype="102" href="https://community.nxp.com/docs/DOC-94961"&gt;https://community.nxp.com/docs/DOC-94961&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The maximum IPU can rotate is 1024x1024. Linux kernel splits the image to show images bigger than 1024x1024.&lt;/P&gt;&lt;P&gt;You can check the file linux/drivers/mxc/ipu3/ipu_device.c about the way it splits. See the "create_split_task" function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Feb 2017 16:56:45 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2017-02-13T16:56:45Z</dc:date>
    <item>
      <title>show to framebuffer from IPU </title>
      <link>https://community.nxp.com/t5/i-MX-Processors/show-to-framebuffer-from-IPU-160/m-p/604333#M91030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, All!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm learning to use IPU to display images in the framebuffer.&lt;BR /&gt;&lt;SPAN&gt;I'm looking at the examples from this repository: &lt;/SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2Frogeriorps%2Fipu-examples%2F" rel="nofollow" target="_blank"&gt;https://github.com/rogeriorps/ipu-examples/&lt;/A&gt;&lt;BR /&gt;Based on these examples (imx6-&amp;gt;rotation-&amp;gt;example1) I have performed a series of tests and I have encountered the following problem.&lt;BR /&gt;The problem I have is that when there is &lt;STRONG&gt;NO rotation&lt;/STRONG&gt; the image is not displayed.&lt;/P&gt;&lt;P&gt;The problem is caused when I&amp;nbsp;call IPU_QUEUE_TASK and the input image is exactly the same of output format. To avoid it if NO rotation I skip&amp;nbsp;&lt;SPAN&gt;call IPU_QUEUE_TASK. Right now I don't get the error but&amp;nbsp;nothing is displayed in the framebuffer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any way to tell IPU to show what it has in its buffer in the framebuffer?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm working with the Udoo Dual board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Kernel 3.14-1.0.x-udoo base&amp;nbsp;&lt;SPAN style="color: #2d2d2d; background-color: #ffffff; font-size: 14px;"&gt;3.14.56 Freescale.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #2d2d2d; font-size: 14px;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #2d2d2d; font-size: 14px;"&gt;Thanks!!!&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336350"&gt;rot_ex1_2.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 10:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/show-to-framebuffer-from-IPU-160/m-p/604333#M91030</guid>
      <dc:creator>alexv</dc:creator>
      <dc:date>2017-02-06T10:40:04Z</dc:date>
    </item>
    <item>
      <title>Re: show to framebuffer from IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/show-to-framebuffer-from-IPU-160/m-p/604334#M91031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;Hi Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rotation and flip is supported by IPU, for examples one can look at&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="94961" data-objecttype="102" href="https://community.nxp.com/docs/DOC-94961"&gt;https://community.nxp.com/docs/DOC-94961&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The maximum IPU can rotate is 1024x1024. Linux kernel splits the image to show images bigger than 1024x1024.&lt;/P&gt;&lt;P&gt;You can check the file linux/drivers/mxc/ipu3/ipu_device.c about the way it splits. See the "create_split_task" function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Feb 2017 16:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/show-to-framebuffer-from-IPU-160/m-p/604334#M91031</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2017-02-13T16:56:45Z</dc:date>
    </item>
  </channel>
</rss>