<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Cannot use mfgtool2-cli on Linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-use-mfgtool2-cli-on-Linux/m-p/603452#M90869</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to burn uboot and kernel to my QWKS-SCMIMX6 rev2 board.&lt;/P&gt;&lt;P&gt;I am using latest mfgtools downloaded from &lt;A class="link-titled" href="http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;Quick Start Board for SCM-i.MX 6DQ|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Observations:&lt;/P&gt;&lt;P&gt;1. I do see the VID/PID of the board with lsusb&lt;/P&gt;&lt;P&gt;2. Tried every legal configuration of SW[2-3] - no influence&lt;/P&gt;&lt;P&gt;3. I've successfully loaded mfg uboot and kernel images with Windows 7 PC and MfgTool2.exe onto the same board and got linux console via serial port (I've got kernel panic at initrc, but thats another story)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MfgToolLibLog.txt contains the following:&lt;/P&gt;&lt;P&gt;ModuleID[2] LevelID[1]: MxHidDevice::Read() Error reading from device 0x-7 with size 1025.&lt;/P&gt;&lt;P&gt;ModuleID[2] LevelID[1]: Failed to read HAB type from ROM!!!&lt;/P&gt;&lt;P&gt;ModuleID[2] LevelID[1]: Failed to initialize memory!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect something wrong with mfgtoolcli and/or libMfgToolLib.so. Did someone successfully loaded mfg uboot and kernel using those mfgTools and linux host machine?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additional info: I've already tried Ubuntu 14.04 and 16.04.&lt;/P&gt;&lt;P&gt;Also, I've found source code for mfgtools at &lt;A class="link-titled" href="https://github.com/NXPmicro/mfgtools" title="https://github.com/NXPmicro/mfgtools"&gt;GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A bit of looking into the code reveals that error comes from libusb: LIBUSB_ERROR_TIMEOUT (-7).&lt;/P&gt;&lt;P&gt;Can someone confirm that libMfgToolLib.so works on any Linux setup with QWKS SCM board?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Jan 2017 14:12:29 GMT</pubDate>
    <dc:creator>erezamir</dc:creator>
    <dc:date>2017-01-10T14:12:29Z</dc:date>
    <item>
      <title>Cannot use mfgtool2-cli on Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-use-mfgtool2-cli-on-Linux/m-p/603452#M90869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to burn uboot and kernel to my QWKS-SCMIMX6 rev2 board.&lt;/P&gt;&lt;P&gt;I am using latest mfgtools downloaded from &lt;A class="link-titled" href="http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;Quick Start Board for SCM-i.MX 6DQ|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Observations:&lt;/P&gt;&lt;P&gt;1. I do see the VID/PID of the board with lsusb&lt;/P&gt;&lt;P&gt;2. Tried every legal configuration of SW[2-3] - no influence&lt;/P&gt;&lt;P&gt;3. I've successfully loaded mfg uboot and kernel images with Windows 7 PC and MfgTool2.exe onto the same board and got linux console via serial port (I've got kernel panic at initrc, but thats another story)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MfgToolLibLog.txt contains the following:&lt;/P&gt;&lt;P&gt;ModuleID[2] LevelID[1]: MxHidDevice::Read() Error reading from device 0x-7 with size 1025.&lt;/P&gt;&lt;P&gt;ModuleID[2] LevelID[1]: Failed to read HAB type from ROM!!!&lt;/P&gt;&lt;P&gt;ModuleID[2] LevelID[1]: Failed to initialize memory!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect something wrong with mfgtoolcli and/or libMfgToolLib.so. Did someone successfully loaded mfg uboot and kernel using those mfgTools and linux host machine?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additional info: I've already tried Ubuntu 14.04 and 16.04.&lt;/P&gt;&lt;P&gt;Also, I've found source code for mfgtools at &lt;A class="link-titled" href="https://github.com/NXPmicro/mfgtools" title="https://github.com/NXPmicro/mfgtools"&gt;GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A bit of looking into the code reveals that error comes from libusb: LIBUSB_ERROR_TIMEOUT (-7).&lt;/P&gt;&lt;P&gt;Can someone confirm that libMfgToolLib.so works on any Linux setup with QWKS SCM board?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2017 14:12:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-use-mfgtool2-cli-on-Linux/m-p/603452#M90869</guid>
      <dc:creator>erezamir</dc:creator>
      <dc:date>2017-01-10T14:12:29Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot use mfgtool2-cli on Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-use-mfgtool2-cli-on-Linux/m-p/603453#M90870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you mean you are trying to execute mfgtool in a linux host?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It has been tested only on Windows.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Mar 2017 15:44:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-use-mfgtool2-cli-on-Linux/m-p/603453#M90870</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2017-03-10T15:44:06Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot use mfgtool2-cli on Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-use-mfgtool2-cli-on-Linux/m-p/603454#M90871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has there been any update on this as I am having the same issues with Ubuntu 16.04&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Oct 2017 10:50:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-use-mfgtool2-cli-on-Linux/m-p/603454#M90871</guid>
      <dc:creator>tommos23</dc:creator>
      <dc:date>2017-10-27T10:50:50Z</dc:date>
    </item>
  </channel>
</rss>