<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.Mx6Q dual display with HDMI and LCD on linux QT in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603447#M90867</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;你好，你的这个问题解决了吗？lvds和hdmi双屏显示同一个内容&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jul 2018 06:06:34 GMT</pubDate>
    <dc:creator>jakiewen</dc:creator>
    <dc:date>2018-07-17T06:06:34Z</dc:date>
    <item>
      <title>i.Mx6Q dual display with HDMI and LCD on linux QT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603443#M90863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi supporter,&lt;/P&gt;&lt;P&gt;My iMx6Q board is runing linux+QT, HDMI and LCD device are connected.&lt;/P&gt;&lt;P&gt;I want to support dual display, and set environment in uboot as follow:&lt;/P&gt;&lt;P&gt;setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb0:dev=lcd,TIANMA050-WVGA@60,bpp=32,if=RGB24 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off ldo_active=on'&lt;/P&gt;&lt;P&gt;LCD can display, but HDMI can't output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I change the environment:&lt;/P&gt;&lt;P&gt;setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=lcd,TIANMA050-WVGA@60,bpp=32,if=RGB24 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off ldo_active=on'&lt;/P&gt;&lt;P&gt;HDMI can output, but LCD can't display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dose it mean that kernel don't support dual display or dual dispaly is implmented by applicantion?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BRs,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Feb 2017 07:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603443#M90863</guid>
      <dc:creator>nickruan</dc:creator>
      <dc:date>2017-02-04T07:48:07Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx6Q dual display with HDMI and LCD on linux QT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603444#M90864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi nick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try procedures described in sect.4.7 Running Linux OS on the target&lt;/P&gt;&lt;P&gt;attached Linux Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 05:09:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603444#M90864</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-06T05:09:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx6Q dual display with HDMI and LCD on linux QT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603445#M90865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igorpadykov,&lt;/P&gt;&lt;P&gt;I found that LCD and HDMI can display the same content as long as HDMI resolution width is less than 1024.&lt;/P&gt;&lt;P&gt;I have also found the corresponding code in kernel/driver/mxc/ipu3/ipu_disp.c as follow:&lt;/P&gt;&lt;P&gt;void _ipu_dmfc_set_wait4eot(struct ipu_soc *ipu, int dma_chan, int width)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;if (width &amp;gt;= HIGH_RESOLUTION_WIDTH) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;if (dma_chan == 23)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;_ipu_dmfc_init(ipu, DMFC_HIGH_RESOLUTION_DP, 0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;else if (dma_chan == 28)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;_ipu_dmfc_init(ipu, DMFC_HIGH_RESOLUTION_DC, 0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; ...&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;HIGH_RESOLUTION_WIDTH equal to 1024 here,&lt;/P&gt;&lt;P&gt;Why do external handler for the width?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BRs,&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 08:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603445#M90865</guid>
      <dc:creator>nickruan</dc:creator>
      <dc:date>2017-02-07T08:26:06Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx6Q dual display with HDMI and LCD on linux QT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603446#M90866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check Table 10. Common kernel boot parameters attached&lt;/P&gt;&lt;P&gt;Release Notes p.21&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 10:25:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603446#M90866</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-07T10:25:26Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx6Q dual display with HDMI and LCD on linux QT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603447#M90867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;你好，你的这个问题解决了吗？lvds和hdmi双屏显示同一个内容&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 06:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603447#M90867</guid>
      <dc:creator>jakiewen</dc:creator>
      <dc:date>2018-07-17T06:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.Mx6Q dual display with HDMI and LCD on linux QT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603448#M90868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi i met the same problem,how can i resolve it?&amp;nbsp;&amp;nbsp;&lt;A href="https://community.nxp.com/thread/480015"&gt;https://community.nxp.com/thread/480015&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Aug 2018 03:10:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-Mx6Q-dual-display-with-HDMI-and-LCD-on-linux-QT/m-p/603448#M90868</guid>
      <dc:creator>jakiewen</dc:creator>
      <dc:date>2018-08-13T03:10:47Z</dc:date>
    </item>
  </channel>
</rss>