<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to use DDR test for i.MX6? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602031#M90583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My goal is to test the DDR memory and verify that things ARE operational, or if there is some issue I need to deal with. I have had intermittent behavior with my SOM (System On Module) PCBA's. &amp;nbsp;It seems that MOST of them work and some have random failures that have links to errors in memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It was stated in another thread - Linked above - that the computer should be the "host PC" and the i.MX6 should be "slave".&lt;/P&gt;&lt;P&gt;I am using Windows 7 professional.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. &amp;nbsp;I boot up from an SD card (My boot loader is also on the SD card) so I made sure that it was not installed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. &amp;nbsp;The OTG side of the cable is connected to the i.MX6 side and USB is connected to the host PC side.&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. I opened the GUI Version 2.52&lt;/P&gt;&lt;P&gt;4. Powered my i.MX6 system&lt;/P&gt;&lt;P&gt;5. My computer recognized that a USB device was connected&lt;/P&gt;&lt;P&gt;6. Within the GUI I loaded the Init Script&lt;/P&gt;&lt;P&gt;7. Clicked Download&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I got data output within the terminal of the GUI. SUCCESS!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am having trouble doing a couple tests. &amp;nbsp;I have not tried the DDR Calibration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Failure to write to an address&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Fail to write address 0x00111110&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;0x0 0x4 0x8 0xC&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;----------------------------------------------------------------------------------------------------------------&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;0x00111110: 0x00000000 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;memory read is done&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Failure to run stress test&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;DDR Stress Test Iteration 1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Current Temperature: 46&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;============================================&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;DDR Freq: 396 MHz&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;t0.1: data is addr test&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Address of failure: 0x10000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Data was: 0x50000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;But pattern should match address &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Error: failed to run stress test!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My settings are:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5627i1EE9A7AFEEE29C88/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The output when I click Download:&lt;/P&gt;&lt;P&gt;My output is as follows:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;============================================&lt;BR /&gt; DDR Stress Test (2.5.2) &lt;BR /&gt; Build: Mar 31 2016, 23:07:26&lt;BR /&gt; Freescale Semiconductor, Inc.&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; Chip ID&lt;BR /&gt;CHIP ID = i.MX6 Dual/Quad (0x63)&lt;BR /&gt;Internal Revision = TO1.2&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; Boot Configuration&lt;BR /&gt;SRC_SBMR1(0x020d8004) = 0x00002040&lt;BR /&gt;SRC_SBMR2(0x020d801c) = 0x2a000001&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;ARM Clock set to 1GHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR configuration&lt;BR /&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;BR /&gt;DDR type is DDR3 &lt;BR /&gt;Data width: 64, bank num: 8&lt;BR /&gt;Row size: 15, col size: 10&lt;BR /&gt;Chip select CSD0 is used &lt;BR /&gt;Density per chip select: 2048MB &lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why am I getting errors when I try to run a Stress test? Why can I not read / write to a memory location?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Oct 2016 16:32:04 GMT</pubDate>
    <dc:creator>matthewcook</dc:creator>
    <dc:date>2016-10-26T16:32:04Z</dc:date>
    <item>
      <title>How to use DDR test for i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602030#M90582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found a link to a DDR test and Calibration but I don't see an instruction on how to use the GUI?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a usage somewhere? Step by step?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jivelink2" href="https://community.nxp.com/docs/DOC-105652" title="https://community.nxp.com/docs/DOC-105652"&gt;https://community.nxp.com/docs/DOC-105652&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So far I have downloaded the Gui Version 2.52 and have loaded a script.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/i.mx6 quad/tg-p"&gt;#i.mx6 quad&lt;/A&gt;‌, &lt;A href="https://community.nxp.com/t5/tag/ddr calibration on imx6 dl/tg-p"&gt;#ddr calibration on imx6 dl&lt;/A&gt;‌, &lt;A href="https://community.nxp.com/t5/tag/ddr calibration/tg-p"&gt;#ddr calibration&lt;/A&gt;‌, &lt;A href="https://community.nxp.com/t5/tag/ddr systems/tg-p"&gt;#ddr systems&lt;/A&gt;‌, &lt;A href="https://community.nxp.com/t5/tag/ddr validation/tg-p"&gt;#ddr validation&lt;/A&gt;‌, &lt;A href="https://community.nxp.com/t5/tag/ddr_stress_tester/tg-p"&gt;#ddr_stress_tester&lt;/A&gt;‌, &lt;A href="https://community.nxp.com/t5/tag/i.mx6 system on module/tg-p"&gt;#i.mx6 system on module&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6182i322200DD72A6E64E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Oct 2016 23:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602030#M90582</guid>
      <dc:creator>matthewcook</dc:creator>
      <dc:date>2016-10-25T23:25:03Z</dc:date>
    </item>
    <item>
      <title>Re: How to use DDR test for i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602031#M90583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My goal is to test the DDR memory and verify that things ARE operational, or if there is some issue I need to deal with. I have had intermittent behavior with my SOM (System On Module) PCBA's. &amp;nbsp;It seems that MOST of them work and some have random failures that have links to errors in memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It was stated in another thread - Linked above - that the computer should be the "host PC" and the i.MX6 should be "slave".&lt;/P&gt;&lt;P&gt;I am using Windows 7 professional.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. &amp;nbsp;I boot up from an SD card (My boot loader is also on the SD card) so I made sure that it was not installed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. &amp;nbsp;The OTG side of the cable is connected to the i.MX6 side and USB is connected to the host PC side.&amp;nbsp;&lt;/P&gt;&lt;P&gt;3. I opened the GUI Version 2.52&lt;/P&gt;&lt;P&gt;4. Powered my i.MX6 system&lt;/P&gt;&lt;P&gt;5. My computer recognized that a USB device was connected&lt;/P&gt;&lt;P&gt;6. Within the GUI I loaded the Init Script&lt;/P&gt;&lt;P&gt;7. Clicked Download&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I got data output within the terminal of the GUI. SUCCESS!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am having trouble doing a couple tests. &amp;nbsp;I have not tried the DDR Calibration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Failure to write to an address&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Fail to write address 0x00111110&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;0x0 0x4 0x8 0xC&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;----------------------------------------------------------------------------------------------------------------&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;0x00111110: 0x00000000 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;memory read is done&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Failure to run stress test&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;DDR Stress Test Iteration 1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Current Temperature: 46&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;============================================&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;DDR Freq: 396 MHz&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;t0.1: data is addr test&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Address of failure: 0x10000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Data was: 0x50000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;But pattern should match address &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Error: failed to run stress test!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My settings are:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5627i1EE9A7AFEEE29C88/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The output when I click Download:&lt;/P&gt;&lt;P&gt;My output is as follows:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;============================================&lt;BR /&gt; DDR Stress Test (2.5.2) &lt;BR /&gt; Build: Mar 31 2016, 23:07:26&lt;BR /&gt; Freescale Semiconductor, Inc.&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; Chip ID&lt;BR /&gt;CHIP ID = i.MX6 Dual/Quad (0x63)&lt;BR /&gt;Internal Revision = TO1.2&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; Boot Configuration&lt;BR /&gt;SRC_SBMR1(0x020d8004) = 0x00002040&lt;BR /&gt;SRC_SBMR2(0x020d801c) = 0x2a000001&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;ARM Clock set to 1GHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR configuration&lt;BR /&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;BR /&gt;DDR type is DDR3 &lt;BR /&gt;Data width: 64, bank num: 8&lt;BR /&gt;Row size: 15, col size: 10&lt;BR /&gt;Chip select CSD0 is used &lt;BR /&gt;Density per chip select: 2048MB &lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why am I getting errors when I try to run a Stress test? Why can I not read / write to a memory location?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Oct 2016 16:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602031#M90583</guid>
      <dc:creator>matthewcook</dc:creator>
      <dc:date>2016-10-26T16:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: How to use DDR test for i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602032#M90584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matt&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check presentation on&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-331528"&gt;https://community.nxp.com/docs/DOC-331528&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;most easy way to debug is to start with testing using jtag debugger&lt;/P&gt;&lt;P&gt;and checking signals with oscilloscope.&lt;/P&gt;&lt;P&gt;For example:&lt;/P&gt;&lt;P&gt;---------------------------&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Address of failure: 0x10000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Data was: 0x50000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;But pattern should match address &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Error: failed to run stress test!!!&lt;/P&gt;&lt;P&gt;-----------------------------&lt;/P&gt;&lt;P&gt;means that ddr address 0x10000000 has problems with&lt;/P&gt;&lt;P&gt;bit 0x40000000 - it could be probably incorrectly driven high&lt;/P&gt;&lt;P&gt;for some reasons.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Oct 2016 23:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602032#M90584</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-26T23:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: How to use DDR test for i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602033#M90585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the link. It was very helpful.&lt;/P&gt;&lt;P&gt;I was able to overcome the 1rst issue I reported. (Failure to write to an address)&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was choosing a random address, which as described in the presentation are not all configurable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Error when&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f;"&gt;&lt;STRONG&gt;Default&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;is selected for DDR Density.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;---------------------------&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Address of failure: 0x10000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Data was: 0x50000000&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;But pattern should match address &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Error: failed to run stress test!!!&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;-----------------------------&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;My setup (When error occurs during DDR Stress Test) is as follows:&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6133i924841EEBF8A0FE4/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;________________________________________________________________________________________________________________________________&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;BUT I CAN GET IT TO WORK SUCCESSFULLY IF I CHANGE THE:&amp;nbsp;&lt;STRONG&gt;DDR_DENSITY&lt;/STRONG&gt; parameter to 1GB&amp;nbsp;&lt;STRONG&gt;BEFORE&lt;/STRONG&gt; I click the&amp;nbsp;&lt;STRONG&gt;DOWNLOAD&lt;/STRONG&gt; button.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;NOTE:&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;I get the same error as before if I use a frequency any LOWER than 400 MHz and ABOVE 475....i.e. The test ran successfully on a sweep of 400 MHz - 475 MHz. but failed at 500 MHz. with the error:&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;DDR Freq: 500 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;t0: memcpy10 SSN x64 test&lt;BR /&gt;Address of bank2 failure: 0x29aeecc8&lt;BR /&gt;Data was: 0xFFFFEFFFFFEFFFFF &lt;BR /&gt;But pattern was: 0xFFFFEFFFFFFFFFFF&lt;BR /&gt;Error: failed to run stress test!!!&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Here is my setup (When &lt;SPAN style="text-decoration: underline;"&gt;No Errors&amp;nbsp;&lt;SPAN style="background-color: #ffffff;"&gt;400 MHz - 475 MHz&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;occur during DDR Stress Test):&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6068i28E58886C589966B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;The memory seems to be reading a 2GB density still, as previously shown in original post.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P&gt;ARM Clock set to 1GHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR configuration&lt;BR /&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;BR /&gt;DDR type is DDR3 &lt;BR /&gt;Data width: 64, bank num: 8&lt;BR /&gt;Row size: 15, col size: 10&lt;BR /&gt;Chip select CSD0 is used &lt;BR /&gt;Density per chip select: 2048MB &lt;BR /&gt;============================================&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P style="border: 0px;"&gt;&lt;/P&gt;&lt;P style="border: 0px;"&gt;Why would the GUI interface have an error when I leave the DDR Density&amp;nbsp;&lt;STRONG&gt;Default&lt;/STRONG&gt; and operate when I choose the DDR Density as&amp;nbsp;&lt;STRONG&gt;1GB &lt;/STRONG&gt;when it reads a Density of 2048?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Is the previous test I ran still valid where it failed? (Indicating I have a problem) ....... [DDR Density set to Default]&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2016 19:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602033#M90585</guid>
      <dc:creator>matthewcook</dc:creator>
      <dc:date>2016-10-28T19:49:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to use DDR test for i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602034#M90586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;from p.5 presentation:&lt;BR /&gt;"The Density information is obtained from the initscript. "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is real density used on your board ? GUI just calculates data&lt;BR /&gt;from your script, if it is wrong please recheck script and enter valid data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Why would the GUI interface have an error when I leave the DDR Density Default and &lt;BR /&gt;&amp;gt;operate when I choose the DDR Density as 1GB when it reads a Density of 2048?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this may be related to : " No Errors 400 MHz - 475 MHz occur during DDR Stress Test"&lt;BR /&gt;- that is some range of memory (address lines) are excluded from test.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please use guideline from p.31 presentation:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"If using DDR3 and if you plan to run calibration, then it is important to fill out the MR1 value, like “0004”."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Oct 2016 00:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602034#M90586</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-29T00:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: How to use DDR test for i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602035#M90587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks. I have been testing different modules using the calibration portion and I believe I have some good values that I have now input into the register programming aid script.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Q.&amp;nbsp;&amp;nbsp;What is real density used on your board ? GUI just calculates data&lt;/SPAN&gt;&lt;BR style="color: #51626f; background-color: #ffffff;" /&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;from your script, if it is wrong please recheck script and enter valid data.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;A. The DDR3 we are using is (&lt;/SPAN&gt;IS43TR16128B-125KBLI-TR). The datasheet shows that it is a size of 2GB. Is that the density?&lt;/P&gt;&lt;P&gt;It is not clear in the script where that is being calculated from. &amp;nbsp;Is there a line I should edit?&lt;/P&gt;&lt;P&gt;I am using the following script:&lt;/P&gt;&lt;P&gt;ddr_stress_tester_v2.60\script\mx6dq\MX6Q_ARD_DDR3_register_programming_aid_v1.5.inc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2016 15:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602035#M90587</guid>
      <dc:creator>matthewcook</dc:creator>
      <dc:date>2016-11-03T15:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to use DDR test for i.MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602036#M90588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;please post this on ddr test page&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://community.freescale.com/docs/DOC-105652" title="https://community.freescale.com/docs/DOC-105652"&gt;https://community.freescale.com/docs/DOC-105652&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;where authors of that tool will look at it and probably try to&lt;/P&gt;&lt;P&gt;improve tool interface/descriptions for better usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Nov 2016 00:14:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-DDR-test-for-i-MX6/m-p/602036#M90588</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-11-04T00:14:38Z</dc:date>
    </item>
  </channel>
</rss>