<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: MIPI camera Image is getting corrupted with higher frequency</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-camera-Image-is-getting-corrupted-with-higher-frequency/m-p/602017#M90579</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In addition to that, I've configured the MIPI CSI for 1 lane configuration and data rate is 1500/700Mbps.&lt;/P&gt;&lt;P&gt;Is there any restriction for this ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Feb 2017 07:12:55 GMT</pubDate>
    <dc:creator>titusstalin</dc:creator>
    <dc:date>2017-02-27T07:12:55Z</dc:date>
    <item>
      <title>MIPI camera Image is getting corrupted with higher frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-camera-Image-is-getting-corrupted-with-higher-frequency/m-p/602016#M90578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;I've connected the MIPI camera to imx6 board and trying to capture the frames from it.&lt;/P&gt;&lt;P&gt;But I am getting corrupted frames when I operate the frequency in higher values (say 700Mbps or 1500Mbps)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I have connected the MIPI exerciser (instead of MIPI camera) to imx6 board and getting the same issue.&lt;/P&gt;&lt;P&gt;Using external frequency I operated the MIPI exerciser with lower frequency then I have got the complete exact picture I've configured.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could be the problem ?&lt;/P&gt;&lt;P&gt;Any configuration I'm missing here ?&lt;/P&gt;&lt;P&gt;Can you please help me on this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Titus S.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 06:53:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-camera-Image-is-getting-corrupted-with-higher-frequency/m-p/602016#M90578</guid>
      <dc:creator>titusstalin</dc:creator>
      <dc:date>2017-02-27T06:53:34Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI camera Image is getting corrupted with higher frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-camera-Image-is-getting-corrupted-with-higher-frequency/m-p/602017#M90579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In addition to that, I've configured the MIPI CSI for 1 lane configuration and data rate is 1500/700Mbps.&lt;/P&gt;&lt;P&gt;Is there any restriction for this ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 07:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-camera-Image-is-getting-corrupted-with-higher-frequency/m-p/602017#M90579</guid>
      <dc:creator>titusstalin</dc:creator>
      <dc:date>2017-02-27T07:12:55Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI camera Image is getting corrupted with higher frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-camera-Image-is-getting-corrupted-with-higher-frequency/m-p/602018#M90580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Titus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6DQ RM sect.37.1.2.1.1 Camera Ports describes it as :&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fref_manual%2FIMX6DQRM.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The maximum bandwidth of the interface is as follows:&lt;BR /&gt;• 200Mhz for 4 data lanes configuration (800Mbps/lane, 400MByte/sec)&lt;BR /&gt;• 187.5Mhz for 3 data lanes configuration (1000Mbps/lane, 375MByte/sec)&lt;BR /&gt;• 125Mhz for 2 data lanes configuration (1000Mbps/lane, 250MByte/sec )&lt;BR /&gt;• 62.5Mhz for 1 data lane configuration (1000Mbps/lane, 125Mbyte/sec)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 08:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-camera-Image-is-getting-corrupted-with-higher-frequency/m-p/602018#M90580</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-27T08:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI camera Image is getting corrupted with higher frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-camera-Image-is-getting-corrupted-with-higher-frequency/m-p/602019#M90581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;How can I configure the MIPI CSI camera driver for number of lanes ?&lt;/P&gt;&lt;P&gt;I've tried to use "mipi_csi2_set_lanes(mipi_csi2_info, 4)" for 4 lanes configuration.&lt;/P&gt;&lt;P&gt;But I am not able to get the frames after this change.&lt;/P&gt;&lt;P&gt;Is there any other change I need to make it for lanes count ?&lt;/P&gt;&lt;P&gt;Can you please us on this ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 09:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-camera-Image-is-getting-corrupted-with-higher-frequency/m-p/602019#M90581</guid>
      <dc:creator>titusstalin</dc:creator>
      <dc:date>2017-02-27T09:19:13Z</dc:date>
    </item>
  </channel>
</rss>