<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I.MX6 SATA problem  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-SATA-problem/m-p/601738#M90527</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, community&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I meet a problem of SATA&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;hardware : &amp;nbsp;Imx6q core board + carrier &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;OS : &amp;nbsp;LINUX 3.0.35 &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;SATA device : &amp;nbsp;I tried &amp;nbsp;both &amp;nbsp;HDD and SSD&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;when power on we can see this information from serial port:&amp;nbsp;&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Uniform Multi-Platform E-IDE driver&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ide-gd driver 1.18&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ahci: SSS flag set, parallel bus scan disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ahci ahci.0: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;scsi0 : ahci_platform&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02200fff] port 0x100 irq 71&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;GPMI NAND driver registered. (IMX)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;.....&lt;/P&gt;&lt;P&gt;and later:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ata1: SATA link down (SStatus 0 SControl 300)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use external power for HDD, so power is stable.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Feb 2017 09:22:36 GMT</pubDate>
    <dc:creator>sunfrank</dc:creator>
    <dc:date>2017-02-04T09:22:36Z</dc:date>
    <item>
      <title>I.MX6 SATA problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-SATA-problem/m-p/601738#M90527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, community&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I meet a problem of SATA&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;hardware : &amp;nbsp;Imx6q core board + carrier &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;OS : &amp;nbsp;LINUX 3.0.35 &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;SATA device : &amp;nbsp;I tried &amp;nbsp;both &amp;nbsp;HDD and SSD&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;when power on we can see this information from serial port:&amp;nbsp;&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Uniform Multi-Platform E-IDE driver&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ide-gd driver 1.18&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ahci: SSS flag set, parallel bus scan disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ahci ahci.0: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;scsi0 : ahci_platform&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02200fff] port 0x100 irq 71&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;GPMI NAND driver registered. (IMX)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;.....&lt;/P&gt;&lt;P&gt;and later:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ata1: SATA link down (SStatus 0 SControl 300)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use external power for HDD, so power is stable.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Feb 2017 09:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-SATA-problem/m-p/601738#M90527</guid>
      <dc:creator>sunfrank</dc:creator>
      <dc:date>2017-02-04T09:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 SATA problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-SATA-problem/m-p/601739#M90528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general for better signal shape one can try to tweak IOMUX GPR13 register.&lt;BR /&gt;IOMUX GPR13 defines various SATA Phy transmitter/receiver settings.&lt;/P&gt;&lt;P&gt;Is it working in uboot, if yes then one can try to change configurations for IOMUXC_GPR13 to be same&lt;BR /&gt;in kernel as in U-boot (helped some customers).&lt;/P&gt;&lt;P&gt;diff --git a/arch/arm/mach-mx6/board-mx6q_sabresd.c b/arch/arm/mach-mx6/board-m&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;index ac9b8f8..95e5f2a 100644&lt;BR /&gt;--- a/arch/arm/mach-mx6/board-mx6q_sabresd.c&lt;BR /&gt;+++ b/arch/arm/mach-mx6/board-mx6q_sabresd.c&lt;BR /&gt;@@ -1177,7 +1177,7 @@ static int mx6q_sabresd_sata_init(struct device *dev, voi&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *.tx_edgerate_0(iomuxc_gpr13[0]),&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; tmpdata = readl(IOMUXC_GPR13);&lt;BR /&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(((tmpdata &amp;amp; ~0x07FFFFFD) | 0x0593A044), IOMUXC_GPR13);&lt;BR /&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(((tmpdata &amp;amp; ~0x07FFFFFD) | 0x0593E4C4), IOMUXC_GPR13);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Feb 2017 23:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-SATA-problem/m-p/601739#M90528</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-05T23:46:13Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 SATA problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-SATA-problem/m-p/601740#M90529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;thank you very much for your reply. &amp;nbsp;my kernal can detect the HDD now,renson is the .config, lack of SATA support. &amp;nbsp; but the new problem is in android 4.4 , still can not detect the HDD, I&amp;nbsp;found a document which says can modify the vold.fstab in ../system/etc,to set the HDD as a SD card. &amp;nbsp;but it seems like vold.fstab is not exsist any more after android 4.4...do you know another way to let android support the sata disk?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 05:55:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-SATA-problem/m-p/601740#M90529</guid>
      <dc:creator>sunfrank</dc:creator>
      <dc:date>2017-02-07T05:55:16Z</dc:date>
    </item>
  </channel>
</rss>