<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6Q-SDB NXP L5 core Android Image got Hangup</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SDB-NXP-L5-core-Android-Image-got-Hangup/m-p/601587#M90481</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;try to set the hdmi again:&lt;/P&gt;&lt;P&gt;Booting with single display: HDMI display&lt;BR /&gt;In the U-Boot prompt, set the U-Boot environment variables as shown below:&lt;BR /&gt;U-Boot &amp;gt; setenv bootcmd boota mmc2&lt;BR /&gt;U-Boot &amp;gt; setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0&lt;BR /&gt;vmalloc=256M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off&lt;BR /&gt;video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=384M&lt;BR /&gt;U-Boot &amp;gt; saveenv&lt;BR /&gt;With the settings above, the Android platform does not start the shell console. It enables the default Android selinux and&lt;BR /&gt;dm_verity security features, which restrict users to change the system and detect the system's information. To avoid this,&lt;BR /&gt;"androidboot.selinux=disabled" and "androidboot.dm_verity=disabled" need to be appended to the U-Boot's bootargs. Boot&lt;BR /&gt;environment variables are as follows:&lt;BR /&gt;U-Boot &amp;gt; setenv bootcmd boota mmc2&lt;BR /&gt;U-Boot &amp;gt; setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0&lt;BR /&gt;vmalloc=256M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off&lt;BR /&gt;video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=384M&lt;BR /&gt;androidboot.selinux=disabled androidboot.dm_verity=disabled&lt;BR /&gt;U-Boot &amp;gt; saveenv&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Apr 2017 08:30:49 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2017-04-17T08:30:49Z</dc:date>
    <item>
      <title>IMX6Q-SDB NXP L5 core Android Image got Hangup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SDB-NXP-L5-core-Android-Image-got-Hangup/m-p/601586#M90480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I flashed L5 core image after Linux kernel got hang-up. Any one can help me to come out this problem .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Serial Port Logs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2014.04-00201-g9d7bf9b (May 05 2015 - 10:14:54)&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.5 at 792 MHz&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Temperature 65 C, calibration data: 0x53d4a47d&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; 1 GiB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;No panel detected: default to Hannstar-XGA&lt;BR /&gt;Display: Hannstar-XGA (1024x768)&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Found PFUZE100 deviceid=10,revid=21&lt;BR /&gt;check_and_clean: reg 0, flag_set 0&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; FEC [PRIME]&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;=&amp;gt; editenv mmcargs&lt;BR /&gt;edit: setenv bootargs console=${console},${baudrate} ${smp} video=mxcfb1:off root=${mmcroot} video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24&lt;BR /&gt;=&amp;gt; saveenv&lt;BR /&gt;Saving Environment to MMC...&lt;BR /&gt;Writing to MMC(1)... done&lt;BR /&gt;=&amp;gt; boot&lt;BR /&gt;booti mmc1&lt;BR /&gt;kernel&amp;nbsp;&amp;nbsp; @ 14008000 (6819456)&lt;BR /&gt;ramdisk&amp;nbsp; @ 15000000 (725617)&lt;BR /&gt;fdt&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; @ 14f00000 (51263)&lt;BR /&gt;kernel cmdline:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; use boot.img command line:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.serialno=051fb9d4e3174029&lt;BR /&gt;switch to ldo_bypass mode!&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Using Device Tree in place at 14f00000, end 14f0f83e&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Printenv Logs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2014.04-00201-g9d7bf9b (May 05 2015 - 10:14:54)&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.5 at 792 MHz&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Temperature 66 C, calibration data: 0x53d4a47d&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; 1 GiB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;No panel detected: default to Hannstar-XGA&lt;BR /&gt;Display: Hannstar-XGA (1024x768)&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Found PFUZE100 deviceid=10,revid=21&lt;BR /&gt;check_and_clean: reg 0, flag_set 0&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; FEC [PRIME]&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;=&amp;gt; printenv&lt;BR /&gt;baudrate=115200&lt;BR /&gt;bootcmd=booti mmc1&lt;BR /&gt;bootdelay=1&lt;BR /&gt;ethact=FEC&lt;BR /&gt;ethaddr=00:04:9f:04:18:5d&lt;BR /&gt;ethprime=FEC&lt;BR /&gt;fastboot_dev=mmc1&lt;BR /&gt;fdt_high=0xffffffff&lt;BR /&gt;initrd_high=0xffffffff&lt;BR /&gt;loadaddr=0x12000000&lt;BR /&gt;mmcargs=setenv bootargs console=${console},${baudrate} ${smp} video=mxcfb1:off root=${mmcroot} video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24&lt;BR /&gt;splashpos=m,m&lt;/P&gt;&lt;P&gt;Environment size: 357/8188 bytes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2017 04:02:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SDB-NXP-L5-core-Android-Image-got-Hangup/m-p/601586#M90480</guid>
      <dc:creator>kumarasamypalan</dc:creator>
      <dc:date>2017-04-12T04:02:06Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q-SDB NXP L5 core Android Image got Hangup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SDB-NXP-L5-core-Android-Image-got-Hangup/m-p/601587#M90481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;try to set the hdmi again:&lt;/P&gt;&lt;P&gt;Booting with single display: HDMI display&lt;BR /&gt;In the U-Boot prompt, set the U-Boot environment variables as shown below:&lt;BR /&gt;U-Boot &amp;gt; setenv bootcmd boota mmc2&lt;BR /&gt;U-Boot &amp;gt; setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0&lt;BR /&gt;vmalloc=256M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off&lt;BR /&gt;video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=384M&lt;BR /&gt;U-Boot &amp;gt; saveenv&lt;BR /&gt;With the settings above, the Android platform does not start the shell console. It enables the default Android selinux and&lt;BR /&gt;dm_verity security features, which restrict users to change the system and detect the system's information. To avoid this,&lt;BR /&gt;"androidboot.selinux=disabled" and "androidboot.dm_verity=disabled" need to be appended to the U-Boot's bootargs. Boot&lt;BR /&gt;environment variables are as follows:&lt;BR /&gt;U-Boot &amp;gt; setenv bootcmd boota mmc2&lt;BR /&gt;U-Boot &amp;gt; setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0&lt;BR /&gt;vmalloc=256M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off&lt;BR /&gt;video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=384M&lt;BR /&gt;androidboot.selinux=disabled androidboot.dm_verity=disabled&lt;BR /&gt;U-Boot &amp;gt; saveenv&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 08:30:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SDB-NXP-L5-core-Android-Image-got-Hangup/m-p/601587#M90481</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-04-17T08:30:49Z</dc:date>
    </item>
  </channel>
</rss>