<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Question, i.MX6SoloX U-Boot with eMMC fastboot enabled</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6SoloX-U-Boot-with-eMMC-fastboot-enabled/m-p/601339#M90397</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, this feature is still not confirmed as being reliably supported in the current versions of software, so, it is not recommended to use it at all.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Mar 2017 08:48:40 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2017-03-06T08:48:40Z</dc:date>
    <item>
      <title>Question, i.MX6SoloX U-Boot with eMMC fastboot enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6SoloX-U-Boot-with-eMMC-fastboot-enabled/m-p/601338#M90396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Let me ask about how to build U-Boot with enabling eMMC Fast boot mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My customer is facing to build u-boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;They want to be sure that the u-boot has a feature for load kernel image with eMMC fastboot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;They found a definition of “CONFIG_FSL_FASTBOOT” in your u-boot source code including your following BSP code. (in mx6sxsabresd.c)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And they think that CONFIG_FSL_FASTBOOT should be defined for u-boot to have a feature to load kernel image with eMMC fastboot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is it true?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Miyamoto&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 05:15:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6SoloX-U-Boot-with-eMMC-fastboot-enabled/m-p/601338#M90396</guid>
      <dc:creator>SLICE</dc:creator>
      <dc:date>2017-02-27T05:15:12Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6SoloX U-Boot with eMMC fastboot enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6SoloX-U-Boot-with-eMMC-fastboot-enabled/m-p/601339#M90397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, this feature is still not confirmed as being reliably supported in the current versions of software, so, it is not recommended to use it at all.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Mar 2017 08:48:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6SoloX-U-Boot-with-eMMC-fastboot-enabled/m-p/601339#M90397</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-03-06T08:48:40Z</dc:date>
    </item>
  </channel>
</rss>