<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SysVinit hang on boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SysVinit-hang-on-boot/m-p/600630#M90265</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I compared the kernel config with the standard linux-imx kernel config and found some differences.&lt;/P&gt;&lt;P&gt;Now it works :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx for help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jan 2017 16:08:58 GMT</pubDate>
    <dc:creator>peterbärtsch</dc:creator>
    <dc:date>2017-01-11T16:08:58Z</dc:date>
    <item>
      <title>SysVinit hang on boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SysVinit-hang-on-boot/m-p/600628#M90263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with init application. When the device reboot (not after power up) sometimes the init hang.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Console output:&lt;/P&gt;&lt;P&gt;Kernel image @ 0x82000000 [ 0x000000 - 0x3dc1f0 ]&lt;BR /&gt;## Flattened Device Tree blob at 88000000&lt;BR /&gt; Booting using the fdt blob at 0x88000000&lt;BR /&gt; Loading Device Tree to 8df21000, end 8df2c0af ... OK&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 1.219227] snvs-secvio 20cc000.caam-snvs: can't get snvs clock&lt;BR /&gt;[ 1.228998] cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)&lt;BR /&gt;INIT: version 2.88 booting&amp;nbsp;&amp;nbsp; &amp;lt;--Now it hangs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When press some keys then it continues boot. I also try to remove all init scripts in rcS folder but the application hangs before it starts the scripts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the imx6sx hw with actual linux-fslc-imx_4.1-1.0.x kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx for help&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2017 10:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SysVinit-hang-on-boot/m-p/600628#M90263</guid>
      <dc:creator>peterbärtsch</dc:creator>
      <dc:date>2017-01-10T10:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: SysVinit hang on boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SysVinit-hang-on-boot/m-p/600629#M90264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the reason may be that WDOG_B pin not connected to external PMIC,&lt;/P&gt;&lt;P&gt;as done in Sabre SD board schematic spf-27392 p.21&lt;/P&gt;&lt;P&gt;Schematics (1)&lt;BR /&gt;i.MX6_SABRE_SDP_DESIGNFILES&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fhardware-development-tools%2Fsabre-development-system%2Fsabre-platform-for-smart-devices-based-on-the-i.mx-6-series%3ARDIMX6SABREPLAT%3Ffpsp%3D1%26tab%3DDesign_Tools_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-platform-for-smart-devices-based-on-the-i.mx-6-series:RDIMX6SABREPLAT?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;For example , in&amp;nbsp;LDO-bypass if just before reboot&amp;nbsp; it is under lowest cpu freq stepoint , but that voltage can not &lt;BR /&gt;make system boot up at default 800MHZ , so there is need use WDOG_B to reset PMIC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2017 23:31:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SysVinit-hang-on-boot/m-p/600629#M90264</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-10T23:31:52Z</dc:date>
    </item>
    <item>
      <title>Re: SysVinit hang on boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SysVinit-hang-on-boot/m-p/600630#M90265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I compared the kernel config with the standard linux-imx kernel config and found some differences.&lt;/P&gt;&lt;P&gt;Now it works :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx for help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2017 16:08:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SysVinit-hang-on-boot/m-p/600630#M90265</guid>
      <dc:creator>peterbärtsch</dc:creator>
      <dc:date>2017-01-11T16:08:58Z</dc:date>
    </item>
  </channel>
</rss>