<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIssues configuring backlight drivers and initializing PWM output from kernel and user space.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issues-configuring-backlight-drivers-and-initializing-PWM-output/m-p/600585#M90239</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having major issues configuring my lcd backlight PWM for the correct configuration. I am using an NXP iMX6 Quad. I have verified that the device tree is correctly configured but I can not even get the PWM to output from the user space control in the terminal window. Also, when I navigate to the back light directory.. cd /sys/class/backlight .....&lt;/P&gt;&lt;P&gt;Has anyone had a similar issues to this or be able to provide any help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Mar 2017 20:16:11 GMT</pubDate>
    <dc:creator>kevinmahlie</dc:creator>
    <dc:date>2017-03-20T20:16:11Z</dc:date>
    <item>
      <title>Issues configuring backlight drivers and initializing PWM output from kernel and user space.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-configuring-backlight-drivers-and-initializing-PWM-output/m-p/600585#M90239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having major issues configuring my lcd backlight PWM for the correct configuration. I am using an NXP iMX6 Quad. I have verified that the device tree is correctly configured but I can not even get the PWM to output from the user space control in the terminal window. Also, when I navigate to the back light directory.. cd /sys/class/backlight .....&lt;/P&gt;&lt;P&gt;Has anyone had a similar issues to this or be able to provide any help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Mar 2017 20:16:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-configuring-backlight-drivers-and-initializing-PWM-output/m-p/600585#M90239</guid>
      <dc:creator>kevinmahlie</dc:creator>
      <dc:date>2017-03-20T20:16:11Z</dc:date>
    </item>
    <item>
      <title>Re: Issues configuring backlight drivers and initializing PWM output from kernel and user space.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-configuring-backlight-drivers-and-initializing-PWM-output/m-p/600586#M90240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the Chapter 47 of the attached document for the information on how to configure and use the PWM and Backlight driver.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Mar 2017 05:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-configuring-backlight-drivers-and-initializing-PWM-output/m-p/600586#M90240</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-03-31T05:12:06Z</dc:date>
    </item>
  </channel>
</rss>