<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CSI parallel camera using  mx6s_capture.ko  on  imx6Q in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CSI-parallel-camera-using-mx6s-capture-ko-on-imx6Q/m-p/600261#M90183</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am porting parallel camera(mt9v034/mt9v032) driver on imx6Q , and the driver for imx6Q(mxc_v4l2_capture) is old using v4l2_int_device, while the mt9v034.c(provided by cmos sensor corp) using v4l2_subdev.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two folders in /drivers/media/platform/mxc, the capture driver is meant for platforms having/using the IPU (i.MX6Q, i.MX6QP, i.MX6DL etc...). Whereas the subdev is targeting the other platforms (i.MX6SL, i.MX6SX, i.MX7 etc...).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to know, if I don't need the IPU, can I just use mx6s_capture.ko and mt9v034.ko on imx6Q ? Are there any extra porting I should do ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Oct 2016 11:33:43 GMT</pubDate>
    <dc:creator>lampo</dc:creator>
    <dc:date>2016-10-25T11:33:43Z</dc:date>
    <item>
      <title>CSI parallel camera using  mx6s_capture.ko  on  imx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-parallel-camera-using-mx6s-capture-ko-on-imx6Q/m-p/600261#M90183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am porting parallel camera(mt9v034/mt9v032) driver on imx6Q , and the driver for imx6Q(mxc_v4l2_capture) is old using v4l2_int_device, while the mt9v034.c(provided by cmos sensor corp) using v4l2_subdev.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two folders in /drivers/media/platform/mxc, the capture driver is meant for platforms having/using the IPU (i.MX6Q, i.MX6QP, i.MX6DL etc...). Whereas the subdev is targeting the other platforms (i.MX6SL, i.MX6SX, i.MX7 etc...).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to know, if I don't need the IPU, can I just use mx6s_capture.ko and mt9v034.ko on imx6Q ? Are there any extra porting I should do ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Oct 2016 11:33:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-parallel-camera-using-mx6s-capture-ko-on-imx6Q/m-p/600261#M90183</guid>
      <dc:creator>lampo</dc:creator>
      <dc:date>2016-10-25T11:33:43Z</dc:date>
    </item>
    <item>
      <title>Re: CSI parallel camera using  mx6s_capture.ko  on  imx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-parallel-camera-using-mx6s-capture-ko-on-imx6Q/m-p/600262#M90184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi glb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mx6s_capture uses CSI/PxP modules, not present in i.MX6Q&lt;/P&gt;&lt;P&gt;so seems this is not possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Oct 2016 11:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-parallel-camera-using-mx6s-capture-ko-on-imx6Q/m-p/600262#M90184</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-25T11:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: CSI parallel camera using  mx6s_capture.ko  on  imx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-parallel-camera-using-mx6s-capture-ko-on-imx6Q/m-p/600263#M90185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;is there any parallel camera driver using v4l2_subdev interface &amp;nbsp;on imx6Q? &amp;nbsp; &amp;nbsp;if not, did I have to modify mt9v034.c back to v4l2_int_device interface, or what can I do ? &amp;nbsp; thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Oct 2016 13:52:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-parallel-camera-using-mx6s-capture-ko-on-imx6Q/m-p/600263#M90185</guid>
      <dc:creator>lampo</dc:creator>
      <dc:date>2016-10-25T13:52:54Z</dc:date>
    </item>
  </channel>
</rss>