<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AC parameters for GPIOs (Vil, Vih, etc) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/AC-parameters-for-GPIOs-Vil-Vih-etc/m-p/600215#M90172</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to verify the AC levels for the GPIOs on i.MX6Q.&lt;/P&gt;&lt;P&gt;The data sheet (rev 4) in chapter 4.7.1 lists the GPIO AC parameters fpr the rise and fall times. But what are the tresholds&amp;nbsp;for high and low? ... as input and output?&lt;/P&gt;&lt;P&gt;&amp;nbsp;In 4.7.2 the AC parameters for DDR in/outputs are listed with Vih, Vil, Vol, Voh , etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What are those values for the GPIOs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ingo Küpper&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Oct 2016 08:15:11 GMT</pubDate>
    <dc:creator>inmaku</dc:creator>
    <dc:date>2016-10-25T08:15:11Z</dc:date>
    <item>
      <title>AC parameters for GPIOs (Vil, Vih, etc)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AC-parameters-for-GPIOs-Vil-Vih-etc/m-p/600215#M90172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to verify the AC levels for the GPIOs on i.MX6Q.&lt;/P&gt;&lt;P&gt;The data sheet (rev 4) in chapter 4.7.1 lists the GPIO AC parameters fpr the rise and fall times. But what are the tresholds&amp;nbsp;for high and low? ... as input and output?&lt;/P&gt;&lt;P&gt;&amp;nbsp;In 4.7.2 the AC parameters for DDR in/outputs are listed with Vih, Vil, Vol, Voh , etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What are those values for the GPIOs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ingo Küpper&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Oct 2016 08:15:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AC-parameters-for-GPIOs-Vil-Vih-etc/m-p/600215#M90172</guid>
      <dc:creator>inmaku</dc:creator>
      <dc:date>2016-10-25T08:15:11Z</dc:date>
    </item>
    <item>
      <title>Re: AC parameters for GPIOs (Vil, Vih, etc)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AC-parameters-for-GPIOs-Vil-Vih-etc/m-p/600216#M90173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For GPIO, the AC threshold parameters are the same as given in the Section 4.6.2 "General Purpose I/O (GPIO) DC Parameters".&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Oct 2016 12:47:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AC-parameters-for-GPIOs-Vil-Vih-etc/m-p/600216#M90173</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-10-25T12:47:27Z</dc:date>
    </item>
  </channel>
</rss>