<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Eth for IMX6SLX in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Eth-for-IMX6SLX/m-p/599996#M90122</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I developed Eth driver on IMX6Quad and it was working but It was not working on IMX6SLX board after I ported it to IMX6SLX. I could control PHY via LEDs under ETH port but it seems the messages were not transmitted out because I saw buffer flag but did not see transmit flag.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you have any ideas to fix this problems? do you have any Eth sample code for IMX6SLX board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Luong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Feb 2017 13:08:19 GMT</pubDate>
    <dc:creator>luongtran</dc:creator>
    <dc:date>2017-02-03T13:08:19Z</dc:date>
    <item>
      <title>Eth for IMX6SLX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Eth-for-IMX6SLX/m-p/599996#M90122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I developed Eth driver on IMX6Quad and it was working but It was not working on IMX6SLX board after I ported it to IMX6SLX. I could control PHY via LEDs under ETH port but it seems the messages were not transmitted out because I saw buffer flag but did not see transmit flag.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you have any ideas to fix this problems? do you have any Eth sample code for IMX6SLX board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Luong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 13:08:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Eth-for-IMX6SLX/m-p/599996#M90122</guid>
      <dc:creator>luongtran</dc:creator>
      <dc:date>2017-02-03T13:08:19Z</dc:date>
    </item>
    <item>
      <title>Re: Eth for IMX6SLX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Eth-for-IMX6SLX/m-p/599997#M90123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at uboot sources&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6sxsabresd/mx6sxsabresd.c?h=imx_v2016.03_4.1.15_2.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6sxsabresd/mx6sxsabresd.c?h=imx_v2016.03_4.1.15_2.0.0_ga"&gt;uboot-imx.git - Freescale i.MX u-boot Tree&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and check attached Linux Manual Chapter 43 FEC Driver&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 23:53:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Eth-for-IMX6SLX/m-p/599997#M90123</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-03T23:53:49Z</dc:date>
    </item>
  </channel>
</rss>