<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: NVCC_SD for eMMC interface</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NVCC-SD-for-eMMC-interface/m-p/599940#M90110</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Surendra&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you are right, one can use VCC_SD to power eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Apr 2017 23:13:05 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-04-11T23:13:05Z</dc:date>
    <item>
      <title>NVCC_SD for eMMC interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NVCC-SD-for-eMMC-interface/m-p/599939#M90109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Currently we are using eMMC memory and its powered through SW1A switcher output of PMIC.&lt;/P&gt;&lt;P&gt;PMIC also supports a dedicated LDO with output called VCC_SD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to reduce load&amp;nbsp;SW1A rail, can I use VCC_SD to power eMMC. Wont it impact the power up/down sequencing of the CPU(i.MX6UL).&lt;/P&gt;&lt;P&gt;Both supply rails are are of 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Surendra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Apr 2017 11:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NVCC-SD-for-eMMC-interface/m-p/599939#M90109</guid>
      <dc:creator>surendrajadhav</dc:creator>
      <dc:date>2017-04-11T11:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: NVCC_SD for eMMC interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NVCC-SD-for-eMMC-interface/m-p/599940#M90110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Surendra&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you are right, one can use VCC_SD to power eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Apr 2017 23:13:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NVCC-SD-for-eMMC-interface/m-p/599940#M90110</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-11T23:13:05Z</dc:date>
    </item>
  </channel>
</rss>