<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Peer to peer connection using broadr reach</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599750#M90048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have created the service request. Kindly provide the required patches and kindly mention how I can apply these patches? Also can I apply these patches for Linaro(Ubuntu) or only for Yocto?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Feb 2017 09:45:58 GMT</pubDate>
    <dc:creator>ajayvenkatakris</dc:creator>
    <dc:date>2017-02-06T09:45:58Z</dc:date>
    <item>
      <title>Peer to peer connection using broadr reach</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599746#M90044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I have two imx6 sabre AI boards with each supporting a BroadR reach PHY card. I have a peer to peer connection in between the boards. I have set up an ip address for both the boards, but while trying to ping between the boards, it says that the network is unreachable. The same set up has worked for the Atheros ENET phy Card. How do I set up the peer to peer connection between the two boards using broadr reach. Both the boards are running linaro Ubuntu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ajay Venkatakrishnan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 10:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599746#M90044</guid>
      <dc:creator>ajayvenkatakris</dc:creator>
      <dc:date>2017-02-03T10:42:49Z</dc:date>
    </item>
    <item>
      <title>Re: Peer to peer connection using broadr reach</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599747#M90045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ajay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please create service request to obtain additional patch&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Feb 2017 23:16:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599747#M90045</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-05T23:16:23Z</dc:date>
    </item>
    <item>
      <title>Re: Peer to peer connection using broadr reach</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599748#M90046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; What is patch required for?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Ajay V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 05:27:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599748#M90046</guid>
      <dc:creator>ajayvenkatakris</dc:creator>
      <dc:date>2017-02-06T05:27:24Z</dc:date>
    </item>
    <item>
      <title>Re: Peer to peer connection using broadr reach</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599749#M90047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one board should be flashed with master (#define BCM89810_MASTER)&lt;BR /&gt;image and the other as slave image. Patch provides necessary definitions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 08:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599749#M90047</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-06T08:13:23Z</dc:date>
    </item>
    <item>
      <title>Re: Peer to peer connection using broadr reach</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599750#M90048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have created the service request. Kindly provide the required patches and kindly mention how I can apply these patches? Also can I apply these patches for Linaro(Ubuntu) or only for Yocto?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 09:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Peer-to-peer-connection-using-broadr-reach/m-p/599750#M90048</guid>
      <dc:creator>ajayvenkatakris</dc:creator>
      <dc:date>2017-02-06T09:45:58Z</dc:date>
    </item>
  </channel>
</rss>