<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: ADB reboot is not working. In Sabre lite?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599580#M90012</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First, can you specify which version of Android you are using? It should be one of Boundary Devices images:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/imx6-builds/" title="https://boundarydevices.com/imx6-builds/"&gt;https://boundarydevices.com/imx6-builds/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I don't understand your log, it seems that you type 'adb reboot' from the Nitrogen serial prompt, this is wrong. In the serial output, just type 'reboot'. The 'adb reboot' command should only be issued from your host PC connected to the SabreLite via USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, 'adb reboot' is tested and working in all our releases since (at least) KitKat.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Oct 2016 10:23:42 GMT</pubDate>
    <dc:creator>gary_bisson</dc:creator>
    <dc:date>2016-10-03T10:23:42Z</dc:date>
    <item>
      <title>ADB reboot is not working. In Sabre lite?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599579#M90011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Log Details:&lt;/P&gt;&lt;P&gt;root@nitrogen6x:/ # adb&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reboot&lt;/P&gt;&lt;P&gt;SysRq : Emergency Remount R/O&lt;BR /&gt;EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)&lt;BR /&gt;EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)&lt;BR /&gt;Emergency Remount complete&lt;BR /&gt;imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!&lt;BR /&gt;reboot: Restarting system with command ''&lt;BR /&gt;mxc_restart: Watchdog reset failed to assert reset&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The display is going to off. but it was unable to restart again itself.&lt;/P&gt;&lt;P&gt;Again i need to start manually.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Oct 2016 09:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599579#M90011</guid>
      <dc:creator>sumanthg</dc:creator>
      <dc:date>2016-10-03T09:14:20Z</dc:date>
    </item>
    <item>
      <title>Re: ADB reboot is not working. In Sabre lite?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599580#M90012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First, can you specify which version of Android you are using? It should be one of Boundary Devices images:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/imx6-builds/" title="https://boundarydevices.com/imx6-builds/"&gt;https://boundarydevices.com/imx6-builds/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I don't understand your log, it seems that you type 'adb reboot' from the Nitrogen serial prompt, this is wrong. In the serial output, just type 'reboot'. The 'adb reboot' command should only be issued from your host PC connected to the SabreLite via USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, 'adb reboot' is tested and working in all our releases since (at least) KitKat.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Oct 2016 10:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599580#M90012</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2016-10-03T10:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: ADB reboot is not working. In Sabre lite?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599581#M90013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;root@nitrogen6x:/ #&amp;nbsp; reboot&lt;/P&gt;&lt;P&gt;SysRq : Emergency Remount R/O&lt;BR /&gt;EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)&lt;BR /&gt;EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)&lt;BR /&gt;Emergency Remount complete&lt;BR /&gt;imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!&lt;BR /&gt;reboot: Restarting system with command ''&lt;BR /&gt;mxc_restart: Watchdog reset failed to assert reset&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;working with Android Marshmallow.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Oct 2016 12:37:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599581#M90013</guid>
      <dc:creator>sumanthg</dc:creator>
      <dc:date>2016-10-03T12:37:31Z</dc:date>
    </item>
    <item>
      <title>Re: ADB reboot is not working. In Sabre lite?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599582#M90014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't reproduce your issue here using the prebuilt image unmodified on a SabreLite rev2 (6-20-13). Please provide the exact version of your board and please mention if you have made any modification (either hw or sw).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a FYI, here is my output:&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;root@nitrogen6x:/ # reboot
SysRq : Emergency Remount R/O
EXT4-fs (mmcblk1p1): re-mounted. Opts: (null)
EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
EXT4-fs (mmcblk1p4): re-mounted. Opts: (null)
EXT4-fs (mmcblk1p6): re-mounted. Opts: (null)
Emergency Remount complete
binder: undelivered transaction 11543
binder: undelivered transaction 11541
imx2-wdt 20bc000.wdog: Device shutdown: Expect reboot!
reboot: Restarting system with command ''
U-Boot 2016.03-20385-ge994090 (Jun 07 2016 - 19:09:13 -0700), Build: jenkins-uboot_v2016.03-56&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Oct 2016 13:44:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599582#M90014</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2016-10-03T13:44:43Z</dc:date>
    </item>
    <item>
      <title>Re: ADB reboot is not working. In Sabre lite?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599583#M90015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi sumanth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please also check that correct board image is used as there are many boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Oct 2016 23:58:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADB-reboot-is-not-working-In-Sabre-lite/m-p/599583#M90015</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-03T23:58:22Z</dc:date>
    </item>
  </channel>
</rss>