<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imxfb: No graphics output until XOrg was started in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187303#M8998</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Both options are still enabled.&lt;/P&gt;&lt;P&gt;The black screen must be another issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is fbcon the module that shows the Tux and boot messages - or show's it only the login prompt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With black screen there is no vsync and hsync signal.&lt;/P&gt;&lt;P&gt;This will enabled first when starting X11.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could be the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Dec 2012 07:56:21 GMT</pubDate>
    <dc:creator>stkoch</dc:creator>
    <dc:date>2012-12-03T07:56:21Z</dc:date>
    <item>
      <title>imxfb: No graphics output until XOrg was started</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187301#M8996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have ported Linux 3.7-rc4 to an board with an i.MX257 CPU. A display is connected via LVDS.&lt;/P&gt;&lt;P&gt;The used distribution is Debian Sqeeze for armel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Until I have started XOrg I have no output on screen, no Linux Tux symbol and no text console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I start XOrg I have a correct output, when I terminate XOrg I have an text console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to show the Linux Tux and/or the Text console before XOrg starts?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The kernel command line includes "video=imxfb:LCD-SVGA-10-4".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is another command line string necessary?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stefan Koch&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Nov 2012 08:52:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187301#M8996</guid>
      <dc:creator>stkoch</dc:creator>
      <dc:date>2012-11-26T08:52:20Z</dc:date>
    </item>
    <item>
      <title>Re: imxfb: No graphics output until XOrg was started</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187302#M8997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm pretty sure that it is a build option for the kernel under drivers-&amp;gt;graphics support-&amp;gt;bootup logo to enable the Tux, and there is another option near there to enable the text console.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Nov 2012 22:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187302#M8997</guid>
      <dc:creator>andrew_questps</dc:creator>
      <dc:date>2012-11-26T22:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: imxfb: No graphics output until XOrg was started</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187303#M8998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Both options are still enabled.&lt;/P&gt;&lt;P&gt;The black screen must be another issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is fbcon the module that shows the Tux and boot messages - or show's it only the login prompt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With black screen there is no vsync and hsync signal.&lt;/P&gt;&lt;P&gt;This will enabled first when starting X11.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could be the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Dec 2012 07:56:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187303#M8998</guid>
      <dc:creator>stkoch</dc:creator>
      <dc:date>2012-12-03T07:56:21Z</dc:date>
    </item>
    <item>
      <title>Re: imxfb: No graphics output until XOrg was started</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187304#M8999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;P&gt;We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2014 06:44:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187304#M8999</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-17T06:44:08Z</dc:date>
    </item>
    <item>
      <title>Re: imxfb: No graphics output until XOrg was started</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187305#M9000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;P&gt;We have not got your response yet and will close the diacussion in 3 days. If you still need help, please feel free to &lt;/P&gt;&lt;P&gt;reply with an update to this discussion.&lt;BR /&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 03:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187305#M9000</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-25T03:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: imxfb: No graphics output until XOrg was started</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187306#M9001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 07:33:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxfb-No-graphics-output-until-XOrg-was-started/m-p/187306#M9001</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-03-03T07:33:39Z</dc:date>
    </item>
  </channel>
</rss>