<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックVideo decoding/rendering pipeline starup delay</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Video-decoding-rendering-pipeline-starup-delay/m-p/598980#M89906</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the imx gstreamer&amp;nbsp;imxvpudec plugin in the context of a video over IP phone. &amp;nbsp;The pipeline it uses to decode and render H.264 video received from the network is written in C but essentially is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; appsrc ! h264parse ! imxvpudec ! imxipuvideotransform !&amp;nbsp;imxg2dvideosink. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code is running on a Boundary Devices BD-SL-I.MX6 which I gather was originally called Sabre Lite and was the original i.MX6 reference design board. &amp;nbsp;The video display device is an HDMI monitor at /dev/video1. &amp;nbsp;The input is from appsrc because packets are coming in via a non-Gstreamer RTP stack. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have log messages when the code sets the pipeline state to PLAY and log messages for pipeline bus events. &amp;nbsp;It seems that from setting the pipeline to PLAY until the state changes from PAUSED to PLAYING takes only about 1 second which is acceptable. &amp;nbsp;But decoded video is not rendered on the HDMI display for nearly 4 seconds from start of receiving packets. &amp;nbsp;&lt;/P&gt;&lt;P&gt;Where might such a long delay most likely arise? &amp;nbsp;Once the video starts rendering the latency is not too terrible. &amp;nbsp;I would estimate it at less than 500 ms. &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Apr 2017 23:31:53 GMT</pubDate>
    <dc:creator>brainmeltdown</dc:creator>
    <dc:date>2017-04-10T23:31:53Z</dc:date>
    <item>
      <title>Video decoding/rendering pipeline starup delay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Video-decoding-rendering-pipeline-starup-delay/m-p/598980#M89906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the imx gstreamer&amp;nbsp;imxvpudec plugin in the context of a video over IP phone. &amp;nbsp;The pipeline it uses to decode and render H.264 video received from the network is written in C but essentially is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; appsrc ! h264parse ! imxvpudec ! imxipuvideotransform !&amp;nbsp;imxg2dvideosink. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code is running on a Boundary Devices BD-SL-I.MX6 which I gather was originally called Sabre Lite and was the original i.MX6 reference design board. &amp;nbsp;The video display device is an HDMI monitor at /dev/video1. &amp;nbsp;The input is from appsrc because packets are coming in via a non-Gstreamer RTP stack. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have log messages when the code sets the pipeline state to PLAY and log messages for pipeline bus events. &amp;nbsp;It seems that from setting the pipeline to PLAY until the state changes from PAUSED to PLAYING takes only about 1 second which is acceptable. &amp;nbsp;But decoded video is not rendered on the HDMI display for nearly 4 seconds from start of receiving packets. &amp;nbsp;&lt;/P&gt;&lt;P&gt;Where might such a long delay most likely arise? &amp;nbsp;Once the video starts rendering the latency is not too terrible. &amp;nbsp;I would estimate it at less than 500 ms. &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Apr 2017 23:31:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Video-decoding-rendering-pipeline-starup-delay/m-p/598980#M89906</guid>
      <dc:creator>brainmeltdown</dc:creator>
      <dc:date>2017-04-10T23:31:53Z</dc:date>
    </item>
    <item>
      <title>Re: Video decoding/rendering pipeline starup delay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Video-decoding-rendering-pipeline-starup-delay/m-p/598981#M89907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The most likely cause of the delay you observe is the fact that the stream decoding can be started only on an I-frame (initial frame), that may appear relatively rare (e.g. once a some seconds) within a stream. The frequency of I-frames appearance depends on the video source side and cannot be improved on the receiving side in any way.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2017 09:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Video-decoding-rendering-pipeline-starup-delay/m-p/598981#M89907</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-04-12T09:53:46Z</dc:date>
    </item>
  </channel>
</rss>