<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Capture on CSI0 in NTSC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Capture-on-CSI0-in-NTSC/m-p/598953#M89902</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have change the VSkip&amp;nbsp;for an even number and it fixe my issue but causes side effect. VScroll does not auto-recover frame position. Any other way to change Odd/Even on the first line or realign interlacing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Guy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Oct 2016 20:00:31 GMT</pubDate>
    <dc:creator>guys_fr</dc:creator>
    <dc:date>2016-10-06T20:00:31Z</dc:date>
    <item>
      <title>Capture on CSI0 in NTSC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-on-CSI0-in-NTSC/m-p/598950#M89899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am investigating and/or questioning myself about the video quality in preview (CE7). I use two different camera (208C 380 lines, OP31 275 lines). I was wandering if CSI input has to be customized for each camera. The encoder is ADV7180 with BT.656 422 standard output. Also, any one&amp;nbsp;of the recommended "fast switching script" hand-up in free running mode&amp;nbsp;(blue screen)!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bosch demystifies analog video resolutions standard in "WhitePaper_enUS_1575840651.pdf". I did not find a way to&amp;nbsp;know&amp;nbsp;lines count.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks. Guy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 15:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-on-CSI0-in-NTSC/m-p/598950#M89899</guid>
      <dc:creator>guys_fr</dc:creator>
      <dc:date>2016-09-30T15:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: Capture on CSI0 in NTSC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-on-CSI0-in-NTSC/m-p/598951#M89900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, I think it' Odd/Even lines issue, validated in graphic drawing tool. How can I test iMX6 changes for Odd/Even in capture / display&amp;nbsp;setting. The DC module have Odd/Even setting. The CPMEM also but always set to "0" in CE7 CPMEM ILVD CF =&amp;nbsp;0. iMX6 Doc.:&lt;/P&gt;&lt;P&gt;40.5.7&amp;nbsp; YUV422: No Odd/Even&lt;BR /&gt;40.5.10 YUV420: Odd line first&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 20:44:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-on-CSI0-in-NTSC/m-p/598951#M89900</guid>
      <dc:creator>guys_fr</dc:creator>
      <dc:date>2016-09-30T20:44:44Z</dc:date>
    </item>
    <item>
      <title>Re: Capture on CSI0 in NTSC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-on-CSI0-in-NTSC/m-p/598952#M89901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for ADV7180 usage in CE7 one can look at&lt;BR /&gt;iMX53_ARD/SRC/DRIVERS/IPUV3/CAMERA/bspcsi.cpp&amp;nbsp; function BSPGetSensorResolution()&lt;BR /&gt;in i.MX53 Windows Embedded Compact 7 Source Code :&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3FcolCode%3DIMX53_WCE700_1105_BSP_SOURCE%26appType%3Dlicense%26location%3Dnull%26fsrch%3D1%26sr%3D1%26Parent_nodeId%3Dfrom%2520search%26Parent_pageType%3Dfrom%2520search%26Parent_nodeId%3D1298573788032723957803%26Parent_pageType%3Dproduct" rel="nofollow" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=IMX53_WCE700_1105_BSP_SOURCE&amp;amp;appType=license&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;Parent_nodeId=from%20search&amp;amp;Parent_pageType=from%20search&amp;amp;Parent_nodeId=1298573788032723957803&amp;amp;Parent_pageType=product&lt;/A&gt;&lt;BR /&gt;ADV7180 operation expalnation for linux can be found on&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/295157"&gt;https://community.nxp.com/thread/295157&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Oct 2016 23:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-on-CSI0-in-NTSC/m-p/598952#M89901</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-02T23:36:54Z</dc:date>
    </item>
    <item>
      <title>Re: Capture on CSI0 in NTSC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-on-CSI0-in-NTSC/m-p/598953#M89902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have change the VSkip&amp;nbsp;for an even number and it fixe my issue but causes side effect. VScroll does not auto-recover frame position. Any other way to change Odd/Even on the first line or realign interlacing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Guy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2016 20:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-on-CSI0-in-NTSC/m-p/598953#M89902</guid>
      <dc:creator>guys_fr</dc:creator>
      <dc:date>2016-10-06T20:00:31Z</dc:date>
    </item>
  </channel>
</rss>