<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Configuring SD card on SPI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-SD-card-on-SPI/m-p/598075#M89756</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are planning to create a custom i.mx6 board with SD card on SPI. We will be using Android 6 as the Operating system.This SD card will not be used for booting but just for external memory.&lt;/P&gt;&lt;P&gt;Is this&amp;nbsp; possible? Also what would be the maximum capacity of the SD Card it would support.&lt;/P&gt;&lt;P&gt;If this is possible&amp;nbsp; then do we have device tree configuration for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Deepika&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Nov 2016 07:03:51 GMT</pubDate>
    <dc:creator>deepika_t</dc:creator>
    <dc:date>2016-11-16T07:03:51Z</dc:date>
    <item>
      <title>Configuring SD card on SPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-SD-card-on-SPI/m-p/598075#M89756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are planning to create a custom i.mx6 board with SD card on SPI. We will be using Android 6 as the Operating system.This SD card will not be used for booting but just for external memory.&lt;/P&gt;&lt;P&gt;Is this&amp;nbsp; possible? Also what would be the maximum capacity of the SD Card it would support.&lt;/P&gt;&lt;P&gt;If this is possible&amp;nbsp; then do we have device tree configuration for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Deepika&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 07:03:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-SD-card-on-SPI/m-p/598075#M89756</guid>
      <dc:creator>deepika_t</dc:creator>
      <dc:date>2016-11-16T07:03:51Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring SD card on SPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-SD-card-on-SPI/m-p/598076#M89757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Deepika&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems SD card on SPI is not supported as shown on below part of document&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10320i6D1221C29D12E121/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 08:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-SD-card-on-SPI/m-p/598076#M89757</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-11-16T08:37:11Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring SD card on SPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-SD-card-on-SPI/m-p/598077#M89758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot Igor for a quick reply. We need to check for SDIO again&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 09:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-SD-card-on-SPI/m-p/598077#M89758</guid>
      <dc:creator>deepika_t</dc:creator>
      <dc:date>2016-11-16T09:40:39Z</dc:date>
    </item>
  </channel>
</rss>