<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Question, i.MX7D TEST_MODE</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597877#M89724</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to ask about TEST_MODE input pin of i.MX7D.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In i.MX7 hardware development guide(IMX7DSHDG, Rev.0), it is mentioned as below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;“The TEST_MODE input is internally connected to an on-chip pulldown device. The user must tie this signal to GND.”&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;On the other hand, TEST_MODE pin is externally pulled-down through 100K ohm register on i.MX7-SABRE board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you show me which is correct?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Actually, my customer made their own i.MX7D board. And they saw clock oscillation did not work when they add the 100K ohm pull-down register. And after removing the 100K ohm, the oscillation worked.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Miyamoto&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Dec 2016 06:02:22 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2016-12-09T06:02:22Z</dc:date>
    <item>
      <title>Question, i.MX7D TEST_MODE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597877#M89724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to ask about TEST_MODE input pin of i.MX7D.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In i.MX7 hardware development guide(IMX7DSHDG, Rev.0), it is mentioned as below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;“The TEST_MODE input is internally connected to an on-chip pulldown device. The user must tie this signal to GND.”&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;On the other hand, TEST_MODE pin is externally pulled-down through 100K ohm register on i.MX7-SABRE board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you show me which is correct?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Actually, my customer made their own i.MX7D board. And they saw clock oscillation did not work when they add the 100K ohm pull-down register. And after removing the 100K ohm, the oscillation worked.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Miyamoto&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 06:02:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597877#M89724</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2016-12-09T06:02:22Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX7D TEST_MODE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597878#M89725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; The TEST_MODE pin should be pulled down. The problem in Your case &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;may be concerned with noisy environment, that requires more strong &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;pulling down. Please try 10 KOhm instead of 100 KOhm for it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 06:19:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597878#M89725</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-12-09T06:19:01Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX7D TEST_MODE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597879#M89726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your prompt reply.&lt;/P&gt;&lt;P&gt;Can I understand that it is better for TEST_MODE pin of i.MX7D to be pulled-down via 100K-10K ohm register rather than direct connection to GND?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 06:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597879#M89726</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2016-12-09T06:26:53Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX7D TEST_MODE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597880#M89727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The TEST_MODE may be connected to GND directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 06:40:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597880#M89727</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-12-09T06:40:17Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX7D TEST_MODE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597881#M89728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand that the direct connection to GND and pull-down are both allowed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 06:54:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX7D-TEST-MODE/m-p/597881#M89728</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2016-12-09T06:54:15Z</dc:date>
    </item>
  </channel>
</rss>