<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6 RGMII RX interface voltage too low in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-RGMII-RX-interface-voltage-too-low/m-p/597713#M89683</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &amp;nbsp;Igor,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thanks for your reply. We found our marvell phy can not provide enough current for the i.mx6.&lt;/P&gt;&lt;P&gt;So we force the speed to 100M and I can ping successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Dec 2016 03:21:49 GMT</pubDate>
    <dc:creator>andy_cc_huang</dc:creator>
    <dc:date>2016-12-15T03:21:49Z</dc:date>
    <item>
      <title>imx6 RGMII RX interface voltage too low</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-RGMII-RX-interface-voltage-too-low/m-p/597711#M89681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;We have a imx6solo custom board and use RGMII + marvell 3.3v phy .&lt;/P&gt;&lt;P&gt;Our circuit is &amp;nbsp; &amp;nbsp; RGMII RX pins + level shifter + marvell&amp;nbsp;phy&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; RGMII TX pins + level shifter + marvell phy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this situation , &amp;nbsp;imx6 tx packets are ok, &amp;nbsp;but RX pins voltage will drop to 2.0v.&lt;/P&gt;&lt;P&gt;And then we remove level shifter , &amp;nbsp; marvell tx come out correct 3.3v &amp;nbsp;after measuring.&lt;/P&gt;&lt;P&gt;In the end , we wired marvell tx + imx6 rx RGMII directly , &amp;nbsp;but the voltage is still drop to 2.0v.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We try our all &amp;nbsp;RX DSE and PUS combination but no help.&lt;/P&gt;&lt;P&gt;Do you have any idea to debug this ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is our pin defination.&lt;/P&gt;&lt;P&gt;pinctrl_enet: enetgrp {&lt;BR /&gt; fsl,pins = &amp;lt;&lt;BR /&gt; MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x1b0b0&lt;BR /&gt; MX6QDL_PAD_KEY_COL2__ENET_MDC 0x1b0b0&lt;BR /&gt; &lt;BR /&gt; MX6QDL_PAD_RGMII_TXC__RGMII_TXC 0x1b0b0&lt;BR /&gt; MX6QDL_PAD_RGMII_TD0__RGMII_TD0 0x1b0b0&lt;BR /&gt; MX6QDL_PAD_RGMII_TD1__RGMII_TD1 0x1b0b0&lt;BR /&gt; MX6QDL_PAD_RGMII_TD2__RGMII_TD2 0x1b0b0&lt;BR /&gt; MX6QDL_PAD_RGMII_TD3__RGMII_TD3 0x1b0b0&lt;BR /&gt; MX6QDL_PAD_RGMII_TX_CTL__RGMII_TX_CTL 0x1b0b0&lt;BR /&gt; &lt;BR /&gt; MX6QDL_PAD_ENET_REF_CLK__ENET_TX_CLK 0x1b0b0&lt;BR /&gt; &lt;BR /&gt; MX6QDL_PAD_RGMII_RXC__RGMII_RXC 0x1b0b0&lt;BR /&gt; MX6QDL_PAD_RGMII_RD0__RGMII_RD0 0x1b0b0&lt;BR /&gt; MX6QDL_PAD_RGMII_RD1__RGMII_RD1 0x1b0b0&lt;BR /&gt; MX6QDL_PAD_RGMII_RD2__RGMII_RD2 0x1b0b0&lt;BR /&gt; MX6QDL_PAD_RGMII_RD3__RGMII_RD3 0x1b0b0 &lt;BR /&gt; MX6QDL_PAD_RGMII_RX_CTL__RGMII_RX_CTL 0x1b0b0&lt;BR /&gt; &lt;BR /&gt; MX6QDL_PAD_GPIO_16__ENET_REF_CLK 0x4001b0a8&lt;BR /&gt; &lt;BR /&gt; &amp;gt;;&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 02:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-RGMII-RX-interface-voltage-too-low/m-p/597711#M89681</guid>
      <dc:creator>andy_cc_huang</dc:creator>
      <dc:date>2016-12-09T02:00:45Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 RGMII RX interface voltage too low</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-RGMII-RX-interface-voltage-too-low/m-p/597712#M89682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this may be hardware related, please check how powered RGMII&lt;/P&gt;&lt;P&gt;pins with oscilloscope using i.MX6SDL Datasheet Table 8. Operating ranges,&lt;/P&gt;&lt;P&gt;Table 96. 21 x 21 mm Functional Contact Assignments&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Just for test one can attach jtag (or printf iomux register) to verify that register&lt;/P&gt;&lt;P&gt;MX6QDL_PAD_RGMII_RD is configured as input.&amp;nbsp; Disconnect input from marvell phy&lt;/P&gt;&lt;P&gt;and configure it as pull-up with PUS, there should be high level with value of RGMII power supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 05:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-RGMII-RX-interface-voltage-too-low/m-p/597712#M89682</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-09T05:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 RGMII RX interface voltage too low</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-RGMII-RX-interface-voltage-too-low/m-p/597713#M89683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &amp;nbsp;Igor,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thanks for your reply. We found our marvell phy can not provide enough current for the i.mx6.&lt;/P&gt;&lt;P&gt;So we force the speed to 100M and I can ping successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 03:21:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-RGMII-RX-interface-voltage-too-low/m-p/597713#M89683</guid>
      <dc:creator>andy_cc_huang</dc:creator>
      <dc:date>2016-12-15T03:21:49Z</dc:date>
    </item>
  </channel>
</rss>