<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SoloX Source Series Resistor LVDS in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SoloX-Source-Series-Resistor-LVDS/m-p/597481#M89636</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does NXP have any recommendations for adding source series resistance to the LVDS output of the SoloX? &amp;nbsp;We would like to slow down the edge rates. &amp;nbsp;We are running the LVDS at 24.58 MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are trying to lower the amount of 688 MHz (LVDS parent clock) noise we are seeing in emissions scans. &amp;nbsp;We were able to add 10 pF 0201 capacitors at each LVDS pair between&amp;nbsp;the vias under the SoloX and see the emissions level go down. &amp;nbsp;But we aren't able to test adding source series resistors because the traces are on internal layers until they reach the connector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use a deserializer (&lt;SPAN style="font-size: 11.0pt;"&gt;DS90CF384&lt;/SPAN&gt;) to drive a RGB parallel LCD on another board with 100 ohm termination resistors for each LVDS pair.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is our LVDS clock tree:&lt;/P&gt;&lt;P&gt;pll5 0 0 688239984 0&lt;BR /&gt; pll5_bypass 0 0 688239984 0&lt;BR /&gt; pll5_video 0 0 688239984 0&lt;BR /&gt; pll5_post_div 0 0 172059996 0&lt;BR /&gt; pll5_video_div 0 0 172059996 0 &lt;BR /&gt; ldb_di0_sel 0 0 172059996 0 &lt;BR /&gt; ldb_di0_div_7 0 0 24579999 0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Sep 2016 14:03:27 GMT</pubDate>
    <dc:creator>scottgauche</dc:creator>
    <dc:date>2016-09-30T14:03:27Z</dc:date>
    <item>
      <title>SoloX Source Series Resistor LVDS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SoloX-Source-Series-Resistor-LVDS/m-p/597481#M89636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does NXP have any recommendations for adding source series resistance to the LVDS output of the SoloX? &amp;nbsp;We would like to slow down the edge rates. &amp;nbsp;We are running the LVDS at 24.58 MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are trying to lower the amount of 688 MHz (LVDS parent clock) noise we are seeing in emissions scans. &amp;nbsp;We were able to add 10 pF 0201 capacitors at each LVDS pair between&amp;nbsp;the vias under the SoloX and see the emissions level go down. &amp;nbsp;But we aren't able to test adding source series resistors because the traces are on internal layers until they reach the connector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use a deserializer (&lt;SPAN style="font-size: 11.0pt;"&gt;DS90CF384&lt;/SPAN&gt;) to drive a RGB parallel LCD on another board with 100 ohm termination resistors for each LVDS pair.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is our LVDS clock tree:&lt;/P&gt;&lt;P&gt;pll5 0 0 688239984 0&lt;BR /&gt; pll5_bypass 0 0 688239984 0&lt;BR /&gt; pll5_video 0 0 688239984 0&lt;BR /&gt; pll5_post_div 0 0 172059996 0&lt;BR /&gt; pll5_video_div 0 0 172059996 0 &lt;BR /&gt; ldb_di0_sel 0 0 172059996 0 &lt;BR /&gt; ldb_di0_div_7 0 0 24579999 0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 14:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SoloX-Source-Series-Resistor-LVDS/m-p/597481#M89636</guid>
      <dc:creator>scottgauche</dc:creator>
      <dc:date>2016-09-30T14:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: SoloX Source Series Resistor LVDS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SoloX-Source-Series-Resistor-LVDS/m-p/597482#M89637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi SCOTT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at LVDS common-mode chokes (represent also resistance)&lt;/P&gt;&lt;P&gt;p.13 SPF-27962 i.MX6SX SabreSD schematic&lt;/P&gt;&lt;P&gt;Schematics (1)&lt;BR /&gt;IMX6SOLOX-SABRESDB-DESIGNFILES&lt;BR /&gt;&lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-6solox-applications-processors:RD-IMX6SX-SABRE?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-6solox-applications-processors:RD-IMX6SX-SABRE?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Oct 2016 00:15:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SoloX-Source-Series-Resistor-LVDS/m-p/597482#M89637</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-01T00:15:50Z</dc:date>
    </item>
  </channel>
</rss>