<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx6ul sim module transmit card command error?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-sim-module-transmit-card-command-error/m-p/596044#M89504</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;Please look at my comments below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;1.&lt;BR /&gt;&amp;nbsp; Section 44.4 (Initialization/Application Information) of i.MX6 UL RM &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;(Rev. 1, 04/2016) provides detailed information how to configure and program the SIM. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;&amp;nbsp; Is Your SIM module I/O interface two-wired or one-wire ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;In the last case some pauses between transfers are reasonable.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;3.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;&amp;nbsp; Is it possible to checkthe basic function of the SIM module with the&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;application mxc_sim_test.out ?&lt;BR /&gt;&lt;BR /&gt;See the following example:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;/unit_tests/mxc_sim_test.out&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;atr[0]= 0x3b atr[1]= 0x68 atr[2]= 0x0 atr[3]= 0x0 atr[4]= 0x0 atr[5]= 0x73 atr[6]= 0xc8&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;atr[7]= 0x40 atr[8]= 0x0 atr[9]= 0x0 atr[10]= 0x90 atr[11]= 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;rx[0] = 0x6e rx[1] = 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;rx[0] = 0x6d rx[1] = 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;rx[0] = 0x6e rx[1] = 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;4.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;You may use the mxc_sim_test as an example.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;The directory below is the directory of the SIM test application source code.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;&amp;lt;Yocto_BuildDir&amp;gt;/linux_test/linuxtest_fsl/linux-test/test/mxc_sim_test&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal"&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Aug 2016 07:21:24 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-08-16T07:21:24Z</dc:date>
    <item>
      <title>imx6ul sim module transmit card command error?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-sim-module-transmit-card-command-error/m-p/596043#M89503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello everyone，when the card response I received, i immediately send a new command to card, but i find the third byte of command is always error.&lt;/P&gt;&lt;P&gt;The last command and new command is about 100us. If i add the time to 200us, the command is sent success. I don't know the driver have problem&lt;/P&gt;&lt;P&gt;or the sim module hardware have problem.Have you encountered this problem？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 Aug 2016 16:04:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-sim-module-transmit-card-command-error/m-p/596043#M89503</guid>
      <dc:creator>kevinliu</dc:creator>
      <dc:date>2016-08-14T16:04:28Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ul sim module transmit card command error?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-sim-module-transmit-card-command-error/m-p/596044#M89504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;Please look at my comments below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;1.&lt;BR /&gt;&amp;nbsp; Section 44.4 (Initialization/Application Information) of i.MX6 UL RM &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;(Rev. 1, 04/2016) provides detailed information how to configure and program the SIM. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;&amp;nbsp; Is Your SIM module I/O interface two-wired or one-wire ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;In the last case some pauses between transfers are reasonable.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;3.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;&amp;nbsp; Is it possible to checkthe basic function of the SIM module with the&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;application mxc_sim_test.out ?&lt;BR /&gt;&lt;BR /&gt;See the following example:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;/unit_tests/mxc_sim_test.out&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;atr[0]= 0x3b atr[1]= 0x68 atr[2]= 0x0 atr[3]= 0x0 atr[4]= 0x0 atr[5]= 0x73 atr[6]= 0xc8&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;atr[7]= 0x40 atr[8]= 0x0 atr[9]= 0x0 atr[10]= 0x90 atr[11]= 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;rx[0] = 0x6e rx[1] = 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;rx[0] = 0x6d rx[1] = 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;rx[0] = 0x6e rx[1] = 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;4.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;You may use the mxc_sim_test as an example.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;The directory below is the directory of the SIM test application source code.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;&amp;lt;Yocto_BuildDir&amp;gt;/linux_test/linuxtest_fsl/linux-test/test/mxc_sim_test&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal"&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 07:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-sim-module-transmit-card-command-error/m-p/596044#M89504</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-08-16T07:21:24Z</dc:date>
    </item>
  </channel>
</rss>