<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6DL SD boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-SD-boot/m-p/595670#M89475</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a custom board used the i.MX6 DualLite and now we can't boot from SD successful. We even can't measure SD_CLK signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tried to change boot mode to serial downloader mode, and use stress test tool v2.52 to read SRC_SBMR1 which value is 0x00000000 and SRC_SBMR2 which value is 0x00000001. The SRC_SBMR2 value is very strange, we have set boot mode to serial downloader mode, bit 24-25 should be 0x01, but when we read it, it 0x00. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have check all BOOT_CFG pins are right, and follow "Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors" chapter 2 and chapter 8, measured the power on sequence, power rail and clock, they all seem OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you give us some ideas?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Dino&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jul 2016 12:00:57 GMT</pubDate>
    <dc:creator>dinochang</dc:creator>
    <dc:date>2016-07-21T12:00:57Z</dc:date>
    <item>
      <title>i.MX6DL SD boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-SD-boot/m-p/595670#M89475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a custom board used the i.MX6 DualLite and now we can't boot from SD successful. We even can't measure SD_CLK signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tried to change boot mode to serial downloader mode, and use stress test tool v2.52 to read SRC_SBMR1 which value is 0x00000000 and SRC_SBMR2 which value is 0x00000001. The SRC_SBMR2 value is very strange, we have set boot mode to serial downloader mode, bit 24-25 should be 0x01, but when we read it, it 0x00. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have check all BOOT_CFG pins are right, and follow "Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors" chapter 2 and chapter 8, measured the power on sequence, power rail and clock, they all seem OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you give us some ideas?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Dino&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 12:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-SD-boot/m-p/595670#M89475</guid>
      <dc:creator>dinochang</dc:creator>
      <dc:date>2016-07-21T12:00:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DL SD boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-SD-boot/m-p/595671#M89476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dino&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check clocks, both 32.768KHz and 24MHz should&lt;/P&gt;&lt;P&gt;operate properly. Also one can try to attach jtag (please use Hardware Development Guide)&lt;/P&gt;&lt;P&gt;and try to run small codes, like toggle pin. Consider possibility to replace processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 00:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-SD-boot/m-p/595671#M89476</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-22T00:39:47Z</dc:date>
    </item>
  </channel>
</rss>