<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Is it possible to use Qt Embedded on Sabre Automative?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595314#M89430</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a few questions : &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) We are trying to compile qt5 with buildroot. We are selecting and compiling configuration files and face no problem but after compilation of uboot,kernel and rootfs and writing down them to SD, board can't detect it. So what are we missing?&lt;/P&gt;&lt;P&gt;2)When I try another uboot, board start the uboot but can't see the kernel. I folllow these steps : &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-99218"&gt;Buildroot for the i.MX6 sabre sd platform in a few commands&lt;/A&gt; &lt;/P&gt;&lt;P&gt;3) We faced same problem about flash to boot on Beaglebone Black. It tried to boot the SD but couldn't achieve. We followed preparing hardware docs on both systems. Can there be a software problem?&lt;/P&gt;&lt;P&gt;4) If we manage to bitbake it, will Qt recognize Sabre automative for direct device deployment, on-device debugging?&lt;/P&gt;&lt;P&gt;5) If it will not be a problem or you, can you show where you got your image for sabre auto?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Jul 2016 05:57:29 GMT</pubDate>
    <dc:creator>bcan</dc:creator>
    <dc:date>2016-07-22T05:57:29Z</dc:date>
    <item>
      <title>Is it possible to use Qt Embedded on Sabre Automative?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595310#M89426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a sabre automative board, I just started to use Qt embedded and used its flash boot to Qt device tool for Sabre SD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I booted SD via this tool and inserted it to board but nothing happened. There is no uboot screen or terminal movement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I doing wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 12:57:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595310#M89426</guid>
      <dc:creator>bcan</dc:creator>
      <dc:date>2016-07-21T12:57:30Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to use Qt Embedded on Sabre Automative?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595311#M89427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bahadir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problably you have a Terminal setup issue, please follow the section 3 of the iMX Linux User Guide document, for download the proper driver to setup with serial terminal. Also verify your Jumper J3 to position SD card in section 4.5.3 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 15:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595311#M89427</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2016-07-21T15:20:18Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to use Qt Embedded on Sabre Automative?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595312#M89428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I managed build in yocto/open embedded linux sameday and got no issue with it. Can't there be another problem? I also tried this code on a linux machine when usb has the Qt image : &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #212121; font-family: wf_segoe-ui_normal, 'Segoe UI', 'Segoe WP', Tahoma, Arial, sans-serif; font-size: 13.3333px;"&gt;lsblk -d&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #212121; font-family: wf_segoe-ui_normal, 'Segoe UI', 'Segoe WP', Tahoma, Arial, sans-serif; font-size: 13.3333px;"&gt;It shows SD with name &lt;SPAN style="color: #212121; font-family: wf_segoe-ui_normal, 'Segoe UI', 'Segoe WP', Tahoma, Arial, sans-serif; font-size: 13.3333px;"&gt;mmcblk0.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 21:07:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595312#M89428</guid>
      <dc:creator>bcan</dc:creator>
      <dc:date>2016-07-21T21:07:14Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to use Qt Embedded on Sabre Automative?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595313#M89429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Short Answer&lt;/STRONG&gt; - Yes, Qt will work on SABRE Automotive board.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Long answer&lt;/STRONG&gt; - The problem that you are facing is not just because of the Qt, but related to your configuration. We are also working on Qt (GPL version )with SABRE Automotive and our custom platforms (based on i.MX6 processors). All are working fine.&lt;/P&gt;&lt;P&gt;You need to '&lt;EM&gt;bitbake&lt;/EM&gt;' the Yocto with &lt;EM&gt;qt5&lt;/EM&gt; and &lt;EM&gt;x11&lt;/EM&gt; backend (windowing system). Then everything will work pretty straight forward.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 04:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595313#M89429</guid>
      <dc:creator>ajithpv</dc:creator>
      <dc:date>2016-07-22T04:59:53Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to use Qt Embedded on Sabre Automative?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595314#M89430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a few questions : &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) We are trying to compile qt5 with buildroot. We are selecting and compiling configuration files and face no problem but after compilation of uboot,kernel and rootfs and writing down them to SD, board can't detect it. So what are we missing?&lt;/P&gt;&lt;P&gt;2)When I try another uboot, board start the uboot but can't see the kernel. I folllow these steps : &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-99218"&gt;Buildroot for the i.MX6 sabre sd platform in a few commands&lt;/A&gt; &lt;/P&gt;&lt;P&gt;3) We faced same problem about flash to boot on Beaglebone Black. It tried to boot the SD but couldn't achieve. We followed preparing hardware docs on both systems. Can there be a software problem?&lt;/P&gt;&lt;P&gt;4) If we manage to bitbake it, will Qt recognize Sabre automative for direct device deployment, on-device debugging?&lt;/P&gt;&lt;P&gt;5) If it will not be a problem or you, can you show where you got your image for sabre auto?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 05:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595314#M89430</guid>
      <dc:creator>bcan</dc:creator>
      <dc:date>2016-07-22T05:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to use Qt Embedded on Sabre Automative?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595315#M89431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; font-size: 14px;"&gt; &lt;/SPAN&gt;&lt;SPAN style="font-size: 12pt;"&gt;&lt;SPAN style="font-weight: bold; font-style: inherit; font-family: inherit;"&gt;&lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="11235" data-objecttype="3" href="https://community.nxp.com/people/Yuri" style="font-weight: inherit; font-style: inherit; font-size: 11.7px; font-family: inherit; color: #017bba;"&gt;Yuri Muhin&lt;/A&gt;​ , &lt;/SPAN&gt;&lt;SPAN style="font-style: inherit; font-family: inherit;"&gt;Could you please help​ him to get Qt working on SABRE platform&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 09:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595315#M89431</guid>
      <dc:creator>ajithpv</dc:creator>
      <dc:date>2016-08-16T09:26:05Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to use Qt Embedded on Sabre Automative?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595316#M89432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; For NXP Yocto BSP (L4.1.15) :&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;$ DISTRO=fsl-imx-fb MACHINE=imx6qsabreauto source fsl-setup-release.sh –b build-fb&lt;/P&gt;&lt;P&gt;$ bitbake fsl-image-qt5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Aug 2016 02:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-use-Qt-Embedded-on-Sabre-Automative/m-p/595316#M89432</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-08-17T02:47:55Z</dc:date>
    </item>
  </channel>
</rss>