<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6Q LDO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-LDO/m-p/595231#M89413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &amp;nbsp;Leonardo Prates,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default the NXP BSP uses the ldo-bypass option which bypasses the internal LDO in the PMU and uses the external PMIC instead. If you will use a NXP board as reference for your design with an external PMIC you may use the ldo-bypass option as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a bit more information on this topic on page 67 of Application Note 4579:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fapp_note%2FAN4579.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/files/32bit/doc/app_note/AN4579.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Sep 2016 21:25:57 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-09-06T21:25:57Z</dc:date>
    <item>
      <title>IMX6Q LDO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-LDO/m-p/595230#M89412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If my board has PMIC, I have to configure:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl,ldo-bypass = &amp;lt;1&amp;gt;;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl,ldo-bypass = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't understand it yet, could someone just answer the option that I have to use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Leonardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 19:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-LDO/m-p/595230#M89412</guid>
      <dc:creator>leonardoprates</dc:creator>
      <dc:date>2016-09-06T19:38:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q LDO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-LDO/m-p/595231#M89413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &amp;nbsp;Leonardo Prates,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default the NXP BSP uses the ldo-bypass option which bypasses the internal LDO in the PMU and uses the external PMIC instead. If you will use a NXP board as reference for your design with an external PMIC you may use the ldo-bypass option as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a bit more information on this topic on page 67 of Application Note 4579:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fapp_note%2FAN4579.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/files/32bit/doc/app_note/AN4579.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 21:25:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-LDO/m-p/595231#M89413</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-09-06T21:25:57Z</dc:date>
    </item>
  </channel>
</rss>