<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imxv4l2src 1280x720 csi camera error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imxv4l2src-1280x720-csi-camera-error/m-p/594411#M89331</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;&amp;nbsp; The messages about IPU_INT_STAT_5 are used to indicate “about errors that are &lt;BR /&gt;result of data rate problems. Such problems may be a result of the IPU running in &lt;BR /&gt;slower clock then required by the use case. This signal can be used in order to indicate &lt;BR /&gt;the system that the IPU can't handle the desired data rate. In that case the system &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;may need to increase the clock to the IPU or simplify the use case.” &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; So, we have here performance problem.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;To improve situation one can apply overlaysink gstreamer element. Please refer to &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;sections 7.5 (Overlaysink usage) and 7.3.1.6.3 (Multiple videos overlay) of “i.MX_Linux_User's_Guide.pdf”. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;Also, please try to increase DMFC FIFO size (dmfc=3 in boot parameter)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType…&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Aug 2016 07:18:37 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-08-17T07:18:37Z</dc:date>
    <item>
      <title>imxv4l2src 1280x720 csi camera error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxv4l2src-1280x720-csi-camera-error/m-p/594410#M89330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use below command to test CSI camera in 1280x720 4.1.15 on and get error as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# gst-launch-1.0 imxv4l2src device=/dev/video0 ! 'video/x-raw,width=1280,height=720,framerate=(fraction)30/1' ! imxv4l2sink&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;====== IMXV4L2SRC: 4.0.9 build on Aug&amp;nbsp; 2 2016 15:43:47. ======&lt;/P&gt;&lt;P&gt;====== IMXV4L2SINK: 4.0.9 build on Aug&amp;nbsp; 2 2016 15:43:47. ======&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;display(/dev/fb0) resolution is (1920x1080).&lt;/P&gt;&lt;P&gt;Pipeline is live and does not need PREROLL ...&lt;/P&gt;&lt;P&gt;Setting pipeline to PLAYING ...&lt;/P&gt;&lt;P&gt;New clock: GstSystemClock&lt;/P&gt;&lt;P&gt;v4l2sink need allocate 3 buffers.&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000&lt;/P&gt;&lt;P&gt;mxc_sdc_fb fb@0: timeout when waiting for flip irq&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000&lt;/P&gt;&lt;P&gt;ERROR: from element /GstPipeline:pipeline0/GstImxV4l2Src:imxv4l2src0: Internal data flow error.&lt;/P&gt;&lt;P&gt;Additional debug info:&lt;/P&gt;&lt;P&gt;/home/mimxc_sdc_fb fb@0: timeout when waiting for flip irq&lt;/P&gt;&lt;P&gt;ke/yocto/imx6qsabresd/tmp/work/coimx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000&lt;/P&gt;&lt;P&gt;rtexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/1.6.0-r0/gstreamer-1.6.0/libs/gst/base/gstbasesrc.c(2943): gst_base_src_loop (): /GstPipeline:pipeline0/GstImxV4l2Src:imxv4l2src0:&lt;/P&gt;&lt;P&gt;streaming task paused, reason error (-5)&lt;/P&gt;&lt;P&gt;Execution ended after 0:00:01.675626667&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;Setting pipeline to READY ...&lt;/P&gt;&lt;P&gt;mxc_sdc_fb fb@0: timeout when waiting for flip irq&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-launch-1.0:908): GStreamer-CRITICAL **: gst_mini_object_unref: assertion 'mini_object-&amp;gt;refcount &amp;gt; 0' failed&lt;/P&gt;&lt;P&gt;Setting pipeline to NULL ...&lt;/P&gt;&lt;P&gt;Total showed frames (5), playing for (0:00:01.676514667), fps (2.982).&lt;/P&gt;&lt;P&gt;Freeing pipeline ...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Aug 2016 09:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxv4l2src-1280x720-csi-camera-error/m-p/594410#M89330</guid>
      <dc:creator>m_c</dc:creator>
      <dc:date>2016-08-12T09:38:22Z</dc:date>
    </item>
    <item>
      <title>Re: imxv4l2src 1280x720 csi camera error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxv4l2src-1280x720-csi-camera-error/m-p/594411#M89331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;&amp;nbsp; The messages about IPU_INT_STAT_5 are used to indicate “about errors that are &lt;BR /&gt;result of data rate problems. Such problems may be a result of the IPU running in &lt;BR /&gt;slower clock then required by the use case. This signal can be used in order to indicate &lt;BR /&gt;the system that the IPU can't handle the desired data rate. In that case the system &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;may need to increase the clock to the IPU or simplify the use case.” &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt; So, we have here performance problem.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;To improve situation one can apply overlaysink gstreamer element. Please refer to &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;sections 7.5 (Overlaysink usage) and 7.3.1.6.3 (Multiple videos overlay) of “i.MX_Linux_User's_Guide.pdf”. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="Normal tm5"&gt;&lt;SPAN class="tm6"&gt;Also, please try to increase DMFC FIFO size (dmfc=3 in boot parameter)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType…&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Aug 2016 07:18:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxv4l2src-1280x720-csi-camera-error/m-p/594411#M89331</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-08-17T07:18:37Z</dc:date>
    </item>
  </channel>
</rss>