<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIpu Initialization</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ipu-Initialization/m-p/594276#M89319</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With i.mx6dl display (ipu and ldb) after initialization, there is nothing on screen until we set these two memory areas with these values: &lt;BR /&gt;*0x02760060=0x00008805; &lt;BR /&gt; *0x02780064=0x0380; &lt;BR /&gt; After writing these values display works properly. In processor reference manual of imx6dl, these memory areas come under the address space of ipu memory mapping which we can not access via ipu registers. Can anyone please describe how can we achieve such settings using ipu registers? we need to have these values for our display to work correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Sep 2016 07:25:22 GMT</pubDate>
    <dc:creator>muhammadasif</dc:creator>
    <dc:date>2016-09-06T07:25:22Z</dc:date>
    <item>
      <title>Ipu Initialization</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ipu-Initialization/m-p/594276#M89319</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With i.mx6dl display (ipu and ldb) after initialization, there is nothing on screen until we set these two memory areas with these values: &lt;BR /&gt;*0x02760060=0x00008805; &lt;BR /&gt; *0x02780064=0x0380; &lt;BR /&gt; After writing these values display works properly. In processor reference manual of imx6dl, these memory areas come under the address space of ipu memory mapping which we can not access via ipu registers. Can anyone please describe how can we achieve such settings using ipu registers? we need to have these values for our display to work correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 07:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ipu-Initialization/m-p/594276#M89319</guid>
      <dc:creator>muhammadasif</dc:creator>
      <dc:date>2016-09-06T07:25:22Z</dc:date>
    </item>
    <item>
      <title>Re: Ipu Initialization</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ipu-Initialization/m-p/594277#M89320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;please look at the following &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/581155"&gt;https://community.nxp.com/message/581155&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 06:44:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ipu-Initialization/m-p/594277#M89320</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-27T06:44:42Z</dc:date>
    </item>
  </channel>
</rss>