<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX 6QP SD Card Boot Problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-6QP-SD-Card-Boot-Problem/m-p/592359#M89219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Janet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;'imx6q-sabresd.dtb' is for other processor i.MX6Q, while&lt;/P&gt;&lt;P&gt;in that case (processor i.MX6QP) naming *.xyzQP" should be used&lt;/P&gt;&lt;P&gt;for example: zImage-imx6qp-sabreauto.dtb e.t.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Oct 2016 23:59:01 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-10-10T23:59:01Z</dc:date>
    <item>
      <title>i.MX 6QP SD Card Boot Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-6QP-SD-Card-Boot-Problem/m-p/592358#M89218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the SABRE board for smart devices&amp;nbsp; 6QP.&amp;nbsp; I need to have the SDcard have the "core-image-base."&lt;/P&gt;&lt;P&gt;I used the Freescale Yocto Project User's Guide, Rev. L_3.14.38_6ul-ga, 09/2015 and successfully build the image and got all the files in ..MYNAME/tmp/deploy/images/imx6qsabresd.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I imaged the SD card as in Section 6.1:&lt;/P&gt;&lt;P&gt;THE DISK UTILITY SHOWS:&amp;nbsp;&amp;nbsp; (Partition 2 has /bin /home, etc.)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5202i8579E49CD627A5AB/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I boot I get the following messages:&lt;/P&gt;&lt;P&gt;*****************************************************************************&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2015.04-imx_v2015.04_3.14.38_6ul_ga+g5d63276 (Sep 05 2016 - 13:43:40)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.5 at 792 MHz&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; Temperature 26 C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; 1 GiB&lt;BR /&gt;PMIC:&amp;nbsp; PFUZE100 ID=0x10&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No panel detected: default to Hannstar-XGA&lt;BR /&gt;Display: Hannstar-XGA (1024x768)&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; FEC [PRIME]&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 0 &lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;reading boot.scr&lt;BR /&gt;** Unable to read file boot.scr **&lt;BR /&gt;reading zImage&lt;BR /&gt;Error reading cluster&lt;BR /&gt;** Unable to read file zImage **&lt;BR /&gt;Booting from net ...&lt;BR /&gt;FEC Waiting for PHY auto negotiation to complete. done&lt;BR /&gt;BOOTP broadcast 1&lt;BR /&gt;BOOTP broadcast 2&lt;BR /&gt;BOOTP broadcast 3&lt;BR /&gt;BOOTP broadcast 4&lt;BR /&gt;DHCP client bound to address 192.168.0.110 (3325 ms)&lt;BR /&gt;Using FEC device&lt;BR /&gt;TFTP from server 0.0.0.0; our IP address is 192.168.0.110; sending through gateway 192.168.0.1&lt;BR /&gt;Filename 'zImage'.&lt;BR /&gt;Load address: 0x12000000&lt;BR /&gt;Loading: *&lt;BR /&gt;TFTP error: 'No such file or directory' (2)&lt;BR /&gt;Not retrying...&lt;BR /&gt;BOOTP broadcast 1&lt;BR /&gt;BOOTP broadcast 2&lt;BR /&gt;DHCP client bound to address 192.168.0.110 (628 ms)&lt;BR /&gt;Using FEC device&lt;BR /&gt;TFTP from server 0.0.0.0; our IP address is 192.168.0.110; sending through gateway 192.168.0.1&lt;BR /&gt;Filename 'imx6q-sabresd.dtb'.&lt;BR /&gt;Load address: 0x18000000&lt;BR /&gt;Loading: *&lt;BR /&gt;TFTP error: 'No such file or directory' (2)&lt;BR /&gt;Not retrying...&lt;BR /&gt;Bad Linux ARM zImage magic!&lt;BR /&gt;=&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;*****************************************************************************&lt;/P&gt;&lt;P&gt;Can anyone help me out?&amp;nbsp;&lt;/P&gt;&lt;P&gt;THANKS IN ADVANCE&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Sep 2016 21:57:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-6QP-SD-Card-Boot-Problem/m-p/592358#M89218</guid>
      <dc:creator>jpe1313</dc:creator>
      <dc:date>2016-09-05T21:57:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 6QP SD Card Boot Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-6QP-SD-Card-Boot-Problem/m-p/592359#M89219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Janet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;'imx6q-sabresd.dtb' is for other processor i.MX6Q, while&lt;/P&gt;&lt;P&gt;in that case (processor i.MX6QP) naming *.xyzQP" should be used&lt;/P&gt;&lt;P&gt;for example: zImage-imx6qp-sabreauto.dtb e.t.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Oct 2016 23:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-6QP-SD-Card-Boot-Problem/m-p/592359#M89219</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-10T23:59:01Z</dc:date>
    </item>
  </channel>
</rss>