<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックYocto: Add/replace file from kernel sources</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Add-replace-file-from-kernel-sources/m-p/591283#M89103</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to replace a file with my version of the file (replace it, not patch) in kernel source and add new file to kernel source. I want to do this during bitbaking my linux image from my custom meta layer. I use github.com/Freescale/linux-fslc.git, branch 4.1-1.0.x-imx kernel and I want to replace and add file in arch/arm/boot/dts. How to do it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Aug 2016 19:56:36 GMT</pubDate>
    <dc:creator>martindusek</dc:creator>
    <dc:date>2016-08-10T19:56:36Z</dc:date>
    <item>
      <title>Yocto: Add/replace file from kernel sources</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Add-replace-file-from-kernel-sources/m-p/591283#M89103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to replace a file with my version of the file (replace it, not patch) in kernel source and add new file to kernel source. I want to do this during bitbaking my linux image from my custom meta layer. I use github.com/Freescale/linux-fslc.git, branch 4.1-1.0.x-imx kernel and I want to replace and add file in arch/arm/boot/dts. How to do it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 19:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Add-replace-file-from-kernel-sources/m-p/591283#M89103</guid>
      <dc:creator>martindusek</dc:creator>
      <dc:date>2016-08-10T19:56:36Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto: Add/replace file from kernel sources</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Add-replace-file-from-kernel-sources/m-p/591284#M89104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin Dusek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You would be using linux-imx as your kernel, from what I understand. The recipes on the BSP Release or Community BSP already use this as the kernel for all the NXP Machines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You would need to change the linux-imx_&amp;lt;VERSION&amp;gt;.bb information on where to obtain the source code. For example for 4.1.15’s BSP would be from linux-imx_4.1.15.bb, which is located on the following path of the BSP Release:&lt;/P&gt;&lt;P&gt;&amp;lt;FSL-RELEASE-BSP &amp;gt;/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/ linux-imx_4.1.15.bb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the device tree you should be able to add the instructions on adding it on the same recipe as it already includes linux-dtb.inc, where the default dtb files are included.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this general guidelines help!&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 23:50:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Add-replace-file-from-kernel-sources/m-p/591284#M89104</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-08-16T23:50:28Z</dc:date>
    </item>
  </channel>
</rss>