<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is ARM domain divider in i.MX6UL? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/What-is-ARM-domain-divider-in-i-MX6UL/m-p/590491#M89076</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp; George Fukutomi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In previous IMX6 family such as 6SL,6SLX, the ARM_CLK_ROOT has s feedback clock path to CCM. This then can be MUXed to CLKO to be observed on a pad, and ARM_CLK_ROOT is after a static /2 divider, which is exactly the ARM domain divider in the pdf.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In 6UL, the ARM_CLK_ROOT is also after a static /2 divider, but the design does not export ARM_CLK_ROOT to CCM, hence we cannot route ARM_CK_ROOT on CLKO on 6UL (please refer to the definition of CCOSR in RM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore, the 6UL’s RM should be updated to change the comment in Figure 18-3. Clock Tree: “clock source goes to ARM Domain and returns to CCM” to “clock source goes to ARM Domain”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please also refer to the thread below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/430464"&gt;i.MX6UL: CCM_CLKO2 arm_clk_root on SD1_DATA2 pad&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jul 2016 20:25:22 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-07-28T20:25:22Z</dc:date>
    <item>
      <title>What is ARM domain divider in i.MX6UL?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-is-ARM-domain-divider-in-i-MX6UL/m-p/590490#M89075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What are 1/2 devider in front of ARM_CLK_ROOT described in the reference manual of MX6UL ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE border="1" class="jiveBorder" height="315" style="border: 1px solid rgb(198, 198, 198); height: 316px; width: 754px;"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TH style="text-align: left; background-color: #f2f2f2; color: #505050; padding: 6px;" valign="middle"&gt;&lt;P&gt;ARM domain divider ?&lt;/P&gt;&lt;/TH&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="padding: 6px;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38388i8571A544645BBD30/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Though described as "clock source goes to ARM Domain and returns to CCM", is possibly this devider for feedback to PLL1?&lt;/P&gt;&lt;P&gt;Because, it seems that this Devider does not exist from actual behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 13:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-is-ARM-domain-divider-in-i-MX6UL/m-p/590490#M89075</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2016-07-20T13:53:51Z</dc:date>
    </item>
    <item>
      <title>Re: What is ARM domain divider in i.MX6UL?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-is-ARM-domain-divider-in-i-MX6UL/m-p/590491#M89076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp; George Fukutomi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In previous IMX6 family such as 6SL,6SLX, the ARM_CLK_ROOT has s feedback clock path to CCM. This then can be MUXed to CLKO to be observed on a pad, and ARM_CLK_ROOT is after a static /2 divider, which is exactly the ARM domain divider in the pdf.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In 6UL, the ARM_CLK_ROOT is also after a static /2 divider, but the design does not export ARM_CLK_ROOT to CCM, hence we cannot route ARM_CK_ROOT on CLKO on 6UL (please refer to the definition of CCOSR in RM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore, the 6UL’s RM should be updated to change the comment in Figure 18-3. Clock Tree: “clock source goes to ARM Domain and returns to CCM” to “clock source goes to ARM Domain”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please also refer to the thread below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/430464"&gt;i.MX6UL: CCM_CLKO2 arm_clk_root on SD1_DATA2 pad&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 20:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-is-ARM-domain-divider-in-i-MX6UL/m-p/590491#M89076</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-07-28T20:25:22Z</dc:date>
    </item>
  </channel>
</rss>